I have an existing project on a 55s06 dev board with a working USART (FLEXCOMM0). I am trying to add an i2c component, FLEXCOMM1, to the build. I have added the component, assigned the pins, and configured the clocks in the configuration tool but the driver code (fsl_i2c.c and fsl_i2c.h) is not generated and I end up with 'include fsl_i2c.h not found' in peripherals.h. I see the calls for I2C_MasterInit() in FLEXCOMM1_Init in peripherals.c, but that will of course fail to link as I2C_MasterInit() is not located anywhere else that I can find
Is there any way to force the regeneration of the driver code? Or is there another way to get the driver code?
I have tried top attach the Mex file but get this error when I try "The attachment's phase2-devkit.mex content type (text/html) does not match its file extension and has been removed."
已解决! 转到解答。
Hello,
I do not know if you try to add the driver, the code driver is not added by the MCUXpresso config tool.
1- In your project click right and then when the popup window appears go to SDK management.
2- In SDK management select the Manage SDK Component another popup windows will appears.
3- Select the option of Drivers [yellow mark].
4- Type the driver you need to add, select and click OK.
If you need more information please let me know.
Best regards,
Pavel