LPC55S16 and config tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC55S16 and config tool

跳至解决方案
3,039 次查看
inventthings
Contributor II

I'm trying to start a new project using SPI on a LPC55S16 in MCUXpresso. I Select pins and peripherals in the Config Tools built into MCUXpresso. However, on the overview screen it says "Tools not supported for the selected processor: Device Configuration".

Under problems tab I can see:

"Processor core 'cm33_core0' detected in MCUXpresso_IDE project does not match with currently selected `core 0`

In addition I see a warning

"Unsupported version of the FLEXCOMM SPI Driver in the toolchain/IDE project. Required 2.01, actual 2.1.1. Project might not compile correctly".

I've checked on MCUXpresso Config Tools|Software Development for NXP Microcontrollers (MCUs) | NXP  and it says

NOTE: Supported devices can be found by visiting the SDK Builder and clicking on "Select Development Board."

I've got the LPC55S16 Dev Kit and it is listed in the SDK Builder.

This is my first project with an NXP device so can someone please help! Thanks.

0 项奖励
回复
1 解答
2,932 次查看
inventthings
Contributor II

I was using (at the time the latest SDK 2.8.0 and MCUXpresso 11.1.1) . Updating with today's newly released MCUXpresso 11.2.0 fixed it.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,933 次查看
inventthings
Contributor II

I was using (at the time the latest SDK 2.8.0 and MCUXpresso 11.1.1) . Updating with today's newly released MCUXpresso 11.2.0 fixed it.

0 项奖励
回复
2,932 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Andrew Robinson ,

Which SDK version do you used ? Please attach your project, I can help you to check.

Please pay attention that, in LPC55s16, we need choose Flexcomm, then config it as SPI in Peripherals view.

Regards,

Alice

0 项奖励
回复