For a KL27 I setup a custom Boot Loader Configuration Area.
Now I'm not understanding how to get Windows to recognize it?
I sent the VID to DEAD and PID to BEEF. The default timeout is five seconds, as is the normal ROM bootloader with no BCA. With USBDeView (View any installed/connected USB device on your system) I see my DEAD BEEF HID device.
The problem is that Windows takes far longer than five seconds to install a new HID device. So it says "Device Unplugged" after five seconds while the driver was being installed. Now I have a device I can not talk too because Windows did not install the DEAD BEEF HID and I can't recover the device (without JTAG like hardware, unit is pain to disassemble due to being water resistant) as the default Freescale VID/PID as been replaced. How do I recover this, other than JTAG?
How is this suppose to work? Any device with an application already loaded and having a short timeout is going to have this problem is it not? What have I missed?