I have the U-boot source from git://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.
I was wondering why for the ls1021a board support (IOT, TWR, QDS, TSN), only the QDS calls erratum_a009942_check_cpo.
I did notice that part of the erratum 9942 is done in the DDR driver.
Cheers,
Renaud
解決済! 解決策の投稿を見る。
Thank you for contacting NXP support!
The errata is board dependent, it's related to the DDR design on board. On ls1021aqds, it uses DDR3L UDIMM/RDIMMs, but on ls1021atwr, it uses DDR3L SDRAM discrete devices. The workaround is needed on ls1021aqds, but not needed on ls1021atwr. As for IOT/TSN board, they're not the mainstream boards included in LSDK release, I didn't use them before, I guess they don't need to apply it.
/*
* This additional workaround of A009942 checks the condition to determine if
* the CPO value set by the existing A009942 workaround needs to be updated.
* If need, print a warning to prompt user reconfigure DDR debug_29[24:31] with
* expected optimal value, the optimal value is highly board dependent.
*/
Thank you for contacting NXP support!
The errata is board dependent, it's related to the DDR design on board. On ls1021aqds, it uses DDR3L UDIMM/RDIMMs, but on ls1021atwr, it uses DDR3L SDRAM discrete devices. The workaround is needed on ls1021aqds, but not needed on ls1021atwr. As for IOT/TSN board, they're not the mainstream boards included in LSDK release, I didn't use them before, I guess they don't need to apply it.
/*
* This additional workaround of A009942 checks the condition to determine if
* the CPO value set by the existing A009942 workaround needs to be updated.
* If need, print a warning to prompt user reconfigure DDR debug_29[24:31] with
* expected optimal value, the optimal value is highly board dependent.
*/