u-boot signing process

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot signing process

1,179 Views
artem_shimko
Contributor II

Hi,

ls1088a rdb, sd boot mode.

I based on Layerscape Linux Distribution POC User Guide Rev. L5.15.71-2.2.0 — 17 February 2023 

Could you please describe how I can sign u-boot binaries manually?

I generate bl2_sd.pbl and fip_uboot.bin (as well as rcw_1600_sd.rcw [without SB_EN =1], rcw_1600_sd.bin and u-boot.bin) due to bitbake qoriq-atf. I know that can generate it as secure, but I need to do it manually. 

As far as I know, for it the uni_sign is used, but I don't understand what is flow.

Am I correct?

  1. ./gen_keys 2048
  2. ./uni_sign --hash input_files/uni_sign/ls2088_1088/sd/input_uboot_secure (to take key.pub hash, the pub key should be in the CST dir)
  3. cp u-boot.bin to the CST dir
  4. ./uni_sign input_files/uni_sign/ls2088_1088/sd/input_uboot_secure (to sing u-boot)

    The input file for both hash and u-boot signing

Spoiler

/* Copyright (c) 2015 Freescale Semiconductor, Inc.
*/

ESBC=1
---------------------------------------------------
# Specify the platform. [Mandatory]
# Choose Platform -
# TRUST 3.0: LS2085
# TRUST 3.1: LS2088, LS1088
PLATFORM=LS1088
---------------------------------------------------
# Entry Point/Image start address field in the header.[Mandatory]
# (default=ADDRESS of first file specified in images)
# Address can be 64 bit
ENTRY_POINT=80400000
---------------------------------------------------
# Specify the Key Information.
# PUB_KEY [Mandatory] Comma Seperated List
# Usage: <srk1.pub> <srk2.pub> .....
PUB_KEY=srk.pub
# KEY_SELECT [Mandatory]
# USAGE (for TRUST 3.x): (between 1 to
KEY_SELECT=1
# PRI_KEY [Mandatory] Single Key Used for Signing
# USAGE: <srk.pri>
PRI_KEY=srk.pri
---------------------------------------------------
# Specify IMAGE, Max 8 images are possible.
# DST_ADDR is required only for Non-PBL Platform. [Mandatory]
# USAGE : IMAGE_NO = {IMAGE_NAME, SRC_ADDR, DST_ADDR}
# Address can be 64 bit
IMAGE_1={u-boot.bin,80400000,ffffffff}
IMAGE_2={,,}
IMAGE_3={,,}
IMAGE_4={,,}
IMAGE_5={,,}
IMAGE_6={,,}
IMAGE_7={,,}
IMAGE_8={,,}
---------------------------------------------------
# Specify OEM AND FSL ID to be populated in header. [Optional]
# e.g FSL_UID_0=11111111
FSL_UID_0=
FSL_UID_1=
OEM_UID_0=
OEM_UID_1=
OEM_UID_2=
OEM_UID_3=
OEM_UID_4=
---------------------------------------------------
# Specify the output file names [Optional].
# Default Values chosen in Tool
OUTPUT_HDR_FILENAME=hdr_uboot.out
IMAGE_HASH_FILENAME=
RSA_SIGN_FILENAME=
---------------------------------------------------
# Specify The Flags. (0 or 1) - [Optional]
MP_FLAG=0
ISS_FLAG=1
LW_FLAG=0
---------------------------------------------------
# Specify VERBOSE as 1, if you want to Display Header Information [Optional]
VERBOSE=1

The u-boot.bin wasn't modified, but I got hdr_uboot.out. 

  1. What should I do to sign normal u-boot?
  2. How can I sign the rcw.bin?
  3. Should I create pbl and fip before signing or I have to sign u-boot and rcw before creation pbl and fip?

Thanks a lot.

0 Kudos
Reply
5 Replies

1,157 Views
Chavira
NXP TechSupport
NXP TechSupport


Thank you for contacting NXP support!

Follow these steps to compile and deploy TF-A binaries (bl2_.pbl) on the required boot mode.

  1. Compile PBL binary from RCW source file
  2. Compile U-Boot binary 
  3. Compile TF-A binaries (bl2_.pbl and fip.bin)

1-COMPILE PBL BINARY FROM RCW SOURCE FILE

You have to create a new directory to compile the binaries that you need to create a TF-A binary

You need to compile the rcw_<boot_mode>.bin binary to build the bl2_<boot_mode>.pbl binary.

 

Clone the rcw repository and compile the PBL binary.

  1. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/rcw
  2. $ cd rcw
  3. $ git checkout -b LSDK-21.08 LSDK-21.08
  4. $ cd <platform>
  5. If required, make changes to the rcw files.
  6. $ make

 

Inside of the directory called “RR_FQPP_1455” you can see some binaries in the with the next nomenclature:

rcw_<freq>.bin

Where “freq” is the frequency in MHz of the processor.

2-COMPILE U-BOOT BINARY 

 

You need to compile the u-boot.bin binary to build the fip.bin binary.

 

Clone the u-boot repository and compile the U-Boot binary for TF-A

 

  1. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/u-boot.git
  2. $ cd u-boot
  3. $ git checkout -b LSDK-21.08 LSDK-21.08
  4. $ export ARCH=arm64
  5. $ export CROSS_COMPILE=aarch64-linux-gnu-
  6. $ make distclean
  7. $ make <platform>_tfa_defconfig
  8. $ make

3 Compile TF-A binaries (bl2_.pbl and fip.bin)

 

  1. $ git clone https://source.codeaurora.org/external/qoriq/qoriq-components/atf
  2. $ cd atf
  3. $ git checkout -b LSDK-21.08 LSDK-21.08
  4. $ export ARCH=arm64
  5. $ export CROSS_COMPILE=aarch64-linux-gnu-

 

The compiled BL2 binaries, bl2.bin and bl2_<boot mode>.pbl are available at atf/build/<platform>/release/.

 

NOTE: For any update in the BL2 source code or RCW binary, the bl2_<boot mode>.pbl binary needs to be recompiled.

3.1 HOW TO COMPILE BL2 BINARY

To build BL2 binary with OPTEE, run this command:

 

$ make PLAT=<platform> bl2 SPD=opteed BOOT_MODE=<boot_mode> BL32=<optee_binary> pbl RCW=<path_to_rcw_binary>/<rcw_binary_for_specific_boot_mode>

 

The compiled BL2 binaries, bl2.bin and bl2_<boot_mode>.pbl are available at atf/build/<platform>/release/. For any update in the BL2 source code or RCW binary, the bl2_<boot_mode>.pbl binary needs to be recompiled.

To compile the BL2 binary without OPTEE:

make PLAT=<platform> bl2 BOOT_MODE=<boot_mode> pbl RCW=<path_to_rcw_binary>/<rcw_binary_for_specific_boot_mode>

 

3.2 HOW TO COMPILE FIP BINARY

To build FIP binary with OPTEE and without trusted board boot, run this command:

 

$ make PLAT=<platform> fip BL33=<path_to_u-boot_binary>/u-boot.bin SPD=opteed  BL32=<path_to_optee_binary>/tee.bin

 

To compile the FIP binary without OPTEE and without trusted board boot:

make PLAT=<platform> fip BL33=<path_to_u-boot_binary>/u-boot.bin

The compiled BL31 and FIP binaries, bl31.bin, fip.bin, are available at atf/build/<platform>/release/. For any update in

the BL31, BL32, or BL33 binaries, the fip.bin binary needs to be recompiled

 

0 Kudos
Reply

1,154 Views
artem_shimko
Contributor II

Thank you, but unfortunately, it is not answer for my questions. All these steps I passed. I need to know how I can sign it .

0 Kudos
Reply

1,124 Views
Chavira
NXP TechSupport
NXP TechSupport

That is a little example to signin images on LS1043ARDB.

Command to generate public/private key pair
./gen_keys SIZE NAME
SIZE refers to size of public key in bits. (Modulus size).
Sizes supported -- 1024, 2048, 4096. The generated keys are in PEM format.


../cst/gen_keys 1024 -p srk.pri -k srk.pub
===============================================================
This product includes software developed by the OpenSSL Project for use in the OpenSSL Toolkit 
This product includes cryptographic software written by Eric Young (eay@cryptsoft.com)
===============================================================
Generated SRK pair stored in :
                PUBLIC KEY srk.pub
                PRIVATE KEY srk.pri


The gen_otpmk utility in the Code Signing Tool can be used to generate a 256b random number and insert the hamming code, or simply perform the hamming code insertion for a user defined 256b.

>./gen_otpmk --help
Usage: ./gen_otpmk <trust_arch> [string]
string : 32 byte string
e.g. gen_otpmk 1 1111111122222222333333334444444455555555666666667777777788888888
>./gen_otpmk 2 1111111122222222333333334444444455555555666666667777777788888888


Code Signing Commands for Images: Create CSF Header

Ls -l input_files/uni_sign/ls1043
total 12
-rw-rw-r-- 3 user_lab user_lab 3490 Jan 27 00:34 input_bootscript_secure
-rw-rw-r-- 3 user_lab user_lab 3537 Jan 27 00:34 input_kernel_secure
-rw-rw-r-- 3 user_lab user_lab 3604 Jan 27 00:34 input_uboot_nor_secure

u-boot Image
./input_files/uni_sign/ls1043/input_uboot_nor_secure
The input fields are specified in input_uboot_secure file. Please ensure that the filename mentioned in the input_uboot_secure is same as copied in the cst directory.
Linux Kernel and Root file system
./input_files/uni_sign/ls1043/input_kernel_secure
kernel-fsl-ls1043a-rdb.dtb-ls1043ardb.itb would be validated form u-boot. The flash address used here is according to the address map of u-boot. Please ensure that filename mentioned in the input_uimage_secure is same as copied in the cst directory.


Boot Script
./input_files/uni_sign/ls1043/input_bootscript_secure
Please make sure that filename mentioned in the bootscript is same as copied in the cst directory

Sign the image with CST tools
$ cd /home/user_lab/Linux-LS1043A-SDK-V0.4-20150826-yocto-RDS-20151209/build_ls1043ardb_release/tmp/sysroots/x86_64-linux/usr/bin/cst
$ ll input_files/uni_sign/ls1043
total 12
-rw-rw-r-- 3 user_lab user_lab 3490 Jan 12 08:27 input_bootscript_secure
-rw-rw-r-- 3 user_lab user_lab 3537 Jan 12 08:27 input_kernel_secure
-rw-rw-r-- 3 user_lab user_lab 3604 Jan 12 08:27 input_uboot_nor_secure
$ vi input_files/uni_sign/ls1043/input_kernel_secure
Modify “IMAGE_1={kernel-fsl-ls1043a-rdb.dtb-ls1043ardb.itb,81000000,ffffffff}”
$ vi input_files/uni_sign/ls1043/input_uboot_nor_secure
Modify “IMAGE_1={u-boot-ls1043ardb.bin,60100000,ffffffff}”
$ vi input_files/uni_sign/ls1043/input_bootscript_secure

Note: bootscript is used when you have chain of trust.

CST tool generates the following SHA-256 hash in a binary hash of hex bytes, not string hash of text!
$./uni_sign --hash input_uboot_secure
./uni_sign --hash input_files/uni_sign/ls1043/input_uboot_nor_secure

 

We have some documents that maybe can be useful, please open a case mentioning me following the link:

Support | NXP Semiconductors

 

you must have a valid NDA to receive that files.

0 Kudos
Reply

1,119 Views
artem_shimko
Contributor II

Thank you for your answer. It is really very helpful information.

1. ./gen_otpmk 2 generates OTPMK fuse values. The  "2" means that target platform is big-endian one. As far as I know, I must swap this values before fusing because I use a little-endian host machine to generate it. Am I correct?

2. Same with SRKH values. Please confirm it.

3. What should I do with RCW?

3.1 How can I sign it? 

3.2 Do I have to sign it before creating .pbl or after?

4.1 FIP file consists at least from BL31 and BL33 (u-boot). Is u-boot signed before creating FIP? 

4.2 Where can I get signed by my key BL31?

Thanks a lot for your help!

0 Kudos
Reply

1,107 Views
Chavira
NXP TechSupport
NXP TechSupport

For RCW should be the same direction for cf the sign it is at the same time as u-boot.bin.

The BL31 is signed on fip.bin in that contains bl31 and bl33.

This is the map for the RCW sign.

Chavira_0-1677861850079.png

 

We have a very explained tutorial for LS1043 but I can't publish that file here, please open a case following the link and mention my name on the case to provide you with the file.

Support | NXP Semiconductors

 

0 Kudos
Reply