When I try to build BlueBox3.0 Linux BSP, there always is error about the expat download

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

When I try to build BlueBox3.0 Linux BSP, there always is error about the expat download

579 次查看
ChenHao41
Contributor II

Hi All,

Now I try to build the Bluebox3.0 Linux BSP, there always is error about the expat download.

 

The detail error is as below:

NOTE: Executing Tasks
WARNING: expat-native-2.2.9-r0 do_fetch: Failed to fetch URL https://downloads.sourceforge.net/expat/expat-2.2.9-RENAMED-VULNERABLE-PLEASE-USE-2.4.1-INSTEAD.tar...., attempting MIRRORS if available
ERROR: expat-native-2.2.9-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AGENT_PID="1228"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/mi/fsl-image-auto/sources/poky/scripts/native-intercept:/home/mi/fsl-image-auto/build_lx2160abluebox3ubuntu/tmp/sysroots-uninative/x86_64-linux/usr/bin:/home/mi/fsl-image-auto/build_lx2160abluebox3ubuntu/tmp/work/x86_64-linux/expat-native/2.2.9-r0/recipe-sysroot-native/usr/bin/tar-native:/home/mi/fsl-image-auto/sources/poky/scripts:/home/mi/fsl-image-auto/build_lx2160abluebox3ubuntu/tmp/work/x86_64-linux/expat-native/2.2.9-r0/recipe-sysroot-native/usr/bin/x86_64-linux:/home/mi/fsl-image-auto/build_lx2160abluebox3ubuntu/tmp/work/x86_64-linux/expat-native/2.2.9-r0/recipe-sysroot-native/usr/bin:/home/mi/fsl-image-auto/build_lx2160abluebox3ubuntu/tmp/work/x86_64-linux/expat-native/2.2.9-r0/recipe-sysroot-native/usr/sbin:/home/mi/fsl-image-auto/build_lx2160abluebox3ubuntu/tmp/work/x86_64-linux/expat-native/2.2.9-r0/recipe-sysroot-native/usr/bin:/home/mi/fsl-image-auto/build_lx2160abluebox3ubuntu/tmp/work/x86_64-linux/expat-native/2.2.9-r0/recipe-sysroot-native/sbin:/home/mi/fsl-image-auto/build_lx2160abluebox3ubuntu/tmp/work/x86_64-linux/expat-native/2.2.9-r0/recipe-sysroot-native/bin:/home/mi/fsl-image-auto/sources/poky/bitbake/bin:/home/mi/fsl-image-auto/build_lx2160abluebox3ubuntu/tmp/hosttools"; export HOME="/home/mi"; /usr/bin/env wget -t 2 -T 30 --passive-ftp --no-check-certificate -P /home/mi/fsl-image-auto/downloads 'https://downloads.sourceforge.net/expat/expat-2.2.9-RENAMED-VULNERABLE-PLEASE-USE-2.4.1-INSTEAD.tar....' --progress=dot -v failed with exit code 4, output:
--2022-11-15 02:50:39-- https://downloads.sourceforge.net/expat/expat-2.2.9-RENAMED-VULNERABLE-PLEASE-USE-2.4.1-INSTEAD.tar....
Resolving downloads.sourceforge.net (downloads.sourceforge.net)... 204.68.111.105
Connecting to downloads.sourceforge.net (downloads.sourceforge.net)|204.68.111.105|:443... connected.
HTTP request sent, awaiting response... 301 Moved Permanently
Location: https://downloads.sourceforge.net/project/expat/expat/2.2.9/expat-2.2.9-RENAMED-VULNERABLE-PLEASE-US... [following]
--2022-11-15 02:50:40-- https://downloads.sourceforge.net/project/expat/expat/2.2.9/expat-2.2.9-RENAMED-VULNERABLE-PLEASE-US...
Reusing existing connection to downloads.sourceforge.net:443.
HTTP request sent, awaiting response... 302 Found
Location: https://altushost-swe.dl.sourceforge.net/project/expat/expat/2.2.9/expat-2.2.9-RENAMED-VULNERABLE-PL... [following]
--2022-11-15 02:50:42-- https://altushost-swe.dl.sourceforge.net/project/expat/expat/2.2.9/expat-2.2.9-RENAMED-VULNERABLE-PL...
Resolving altushost-swe.dl.sourceforge.net (altushost-swe.dl.sourceforge.net)... 79.142.76.130
Connecting to altushost-swe.dl.sourceforge.net (altushost-swe.dl.sourceforge.net)|79.142.76.130|:443... failed: Connection timed out.
Retrying.

--2022-11-15 02:51:13-- (try: 2) https://altushost-swe.dl.sourceforge.net/project/expat/expat/2.2.9/expat-2.2.9-RENAMED-VULNERABLE-PL...
Connecting to altushost-swe.dl.sourceforge.net (altushost-swe.dl.sourceforge.net)|79.142.76.130|:443... failed: Connection timed out.
Giving up.


ERROR: expat-native-2.2.9-r0 do_fetch: Fetcher failure for URL: 'https://downloads.sourceforge.net/expat/expat-2.2.9-RENAMED-VULNERABLE-PLEASE-USE-2.4.1-INSTEAD.tar....'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/mi/fsl-image-auto/build_lx2160abluebox3ubuntu/tmp/work/x86_64-linux/expat-native/2.2.9-r0/temp/log.do_fetch.14473
ERROR: Task (virtual:native:/home/mi/fsl-image-auto/sources/poky/meta/recipes-core/expat/expat_2.2.9.bb:do_fetch) failed with exit code '1'
WARNING: libxml2-native-2.9.10-r0 do_fetch: Failed to fetch URL http://www.w3.org/XML/Test/xmlts20080827.tar.gz;subdir=libxml2-2.9.10;name=testtar, attempting MIRRORS if available

It seems that the version of expat is not right. How can I fix the issue?

 

Please see more detail info in the attached log file.

Best Regards

标记 (1)
0 项奖励
回复
1 回复

527 次查看
khushbur
NXP TechSupport
NXP TechSupport

Hi @ChenHao41 

I just tried


wget -t 2 -T 30 --passive-ftp --no-check-certificate -P /home/khushbu/Documents 'https://downloads.sourceforge.net/expat/expat-2.2.9-RENAMED-VULNERABLE-PLEASE-USE-2.4.1-INSTEAD.tar....' --progress=dot -v

Screenshot from 2022-11-18 18-35-07.png

It's looks like working.

There  might be a internet connectivity issue at your side.

Thanks

Khushbu

0 项奖励
回复