SERDES GEN 3 Speeds

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SERDES GEN 3 Speeds

1,405件の閲覧回数
vanlandingham10
Contributor II

The Ref man states that:

"PCIe Gen 3 speed support requires switching to second PLL so when Gen 3 is used
both SerDes PLL will be used by PCIe protocol."

 

Does this mean if I intend on using config 5577 for SERDES PORT 2 That I need to provide two separate external 100 MHZ refclks or can I just provide 1 external 100 MHz refclk and configure the internal mux to re-direct the 2nd pll to use the same external refclk?

 

0 件の賞賛
返信
6 返答(返信)

1,399件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @vanlandingham10 

Which specific processor are you referring to?

Regards,
Mrudang Shelat

 

0 件の賞賛
返信

1,392件の閲覧回数
vanlandingham10
Contributor II

sorry the LS1046

0 件の賞賛
返信

1,404件の閲覧回数
vanlandingham10
Contributor II

I'd like to configure the SERDES ports to support 5577 and 1133. Will my clock scheme work?

 

vanlandingham10_0-1665003409286.jpeg

 

0 件の賞賛
返信

1,384件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @vanlandingham10,

 

The clocking scheme looks fine.

 

Regards,
Mrudang Shelat

0 件の賞賛
返信

1,369件の閲覧回数
vanlandingham10
Contributor II

Okay so If SERDES2 is entirely used for pcie gen3 I can pass a single reference clock to each pll via the internal mux ?

0 件の賞賛
返信

1,321件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi

 

Yes, you can configure SD2_REF_CLK1/SD2_REF_CLK1_B to both the PLL.

 

Regards,
Mrudang Shelat

0 件の賞賛
返信