platform: LX2080a
ddr4: MT40A512M16JY ,8Gb, x16 width
I program the bl2_flexspi_nor.pbl, fip_uboot.bin, fip_ddr_all.bin on the specific address。
The following print appears when my board is power on。What causes DDR PHY to fail ?
i have Defined macro “CONFIG_STATIC_DDR” in plat/nxp/<SOC>/<BOARD>/plafform_def.h to enable discrete DDR timings.
NOTICE: BL2: v2.3():v2.3-LSDK-20.12-dirty
NOTICE: BL2: Built : 18:47:53, May 7 2021
twopass=0
PHY handshake timeout..., ddr_dsr2 = 0
ERROR: Found training error(s): 0x100
ERROR: Error: Waiting for D_INIT timeout.
ERROR: Writing DDR register(s) failed
ERROR: Programing DDRC error
ERROR: DDR init failed.
NOTICE: Incorrect DRAM0 size is defined in platform_def.h
Please refer to the attached QCVS DDRv user manual.
Please configure "Properties" panel according to your DDR data sheet, then generate the initial DDR controller configuration parameter. Then you need to connect DDRv tool to your target board to optimize and validate these DDR configuration parameters.
Would you please open CCS(CodeWarrior Connection Server) console, type "log v" command, then connect to the target board again? The low level CCS log will be printed. Please capture the CCS log and attach it to this thread.
Would you please provide Error capture registers values?
You need to modify "const struct ddr_cfg_regs static_1600" in atf/plat/nxp/<SOC>/<BOARD>/ddr_init.c according to the DDR on your target board.
You could use QCVS DDRv tool to assist you to calculate DDR controller configuration parameters and optimize them.
I configured the above values based on the hardware's CLK To DQS parameters, and then generated the code in CodeWarrior, i Copy the static_1600 to my source code
const struct ddr_cfg_regs static_1600 = {
.cs[0].config = 0x80010412,
.cs[0].bnds = 0xFF,
.sdram_cfg[0] = 0x65240000,
.sdram_cfg[1] = 0x00401030,
.timing_cfg[0] = 0x8055000C,
.timing_cfg[1] = 0x0A0E0C42,
.timing_cfg[2] = 0x0048D11C,
.timing_cfg[3] = 0x11511000,
.timing_cfg[4] = 0x01,
.timing_cfg[5] = 0x05401400,
.timing_cfg[7] = 0x23340000,
.timing_cfg[8] = 0x07116600,
.sdram_mode[0] = 0x01010234,
.sdram_mode[9] = 0x0701,
.sdram_mode[8] = 0x00,
.sdram_mode[2] = 0x00,
.sdram_mode[10] = 0x04000000,
.sdram_mode[11] = 0x00,
.sdram_mode[4] = 0x00,
.sdram_mode[12] = 0x00,
.sdram_mode[13] = 0x00,
.sdram_mode[6] = 0x00,
.sdram_mode[14] = 0x00,
.sdram_mode[15] = 0x00,
.interval = 0x18600618,
.zq_cntl = 0x8A090705,
.wrlvl_cntl[0] = 0x00,
.wrlvl_cntl[1] = 0x00,
.wrlvl_cntl[2] = 0x00,
.debug[28] = 0x01080F70
};
After compiling with the flex-builder -c atf -m lx2160ardb_rev2 -b xspi command, bl2_flexspi_nor.pbl and fip_uboot.bin,programmed it to the Flash, but it still prompts the 2D Training .(I turned on the Debug switch).Debugging several days, all the time not to the main point
The following is the log information, looking forward to your reply...
NOTICE: BL2: v2.3():v2.3-LSDK-20.12-dirty
NOTICE: BL2: Built : 16:15:55, May 18 2021
platform clock 800000000
DDR PLL1 1600000000
DDR PLL2 1600000000
frequency = 800MHz
Vref_phy = 75 percent
Initializing input adv data structure
mr[0] = 0x234
mr[1] = 0x101
mr[2] = 0x0
mr[3] = 0x0
mr[4] = 0x0
mr[5] = 0x0
mr[6] = 0x0
input->cs_d0 = 0x3
input->cs_d1 = 0x0
input->mirror = 0x0
PHY ODT impedance = 48 ohm
PHY DQ driver impedance = 28 ohm
PHY Addr driver impedance = 30 ohm
odt[0] = 0x1
odt[1] = 0x0
odt[2] = 0x0
odt[3] = 0x0
Initializing message block
msg_blk->dram_type = 0x2
msg_blk->sequence_ctrl = 0x31f
msg_blk->phy_cfg = 0x0
msg_blk->x16present = 0x3
msg_blk->dramfreq = 0x640
msg_blk->pll_bypass_en = 0x0
msg_blk->dfi_freq_ratio = 0x2
msg_blk->phy_odt_impedance = 0x0
msg_blk->phy_drv_impedance = 0x0
msg_blk->bpznres_val = 0x0
msg_blk->enabled_dqs = 0x48
msg_blk->acsm_odt_ctrl0 = 0x1
msg_blk->acsm_odt_ctrl1 = 0x0
msg_blk->acsm_odt_ctrl2 = 0x0
msg_blk->acsm_odt_ctrl3 = 0x0
rx2d_train_opt 0, tx2d_train_opt 0
Initialize PHY 0 config
pll_ctrl2 = 0xb
SOC_SI_REV = 2
dll_lck_param = 0x212
dll_gain_ctl = 0x61
acx4_anib_Dis 0x0
Load 1D firmware
Loaded Imaged id 32 of size 6bd0 at address 18003000
Loaded Imaged id 34 of size 6d0 at address 18003000
Execute firmware
Applying PLL optimal settings
pll_ctrl2 = 0xb
pll_ctrl1 = 0x21
pll_test_mode = 0x24
pll_ctrl4 = 0x17f
End of fine write leveling
1D Training completed
Error - Invalid cs_in_use value 0
CDD rrmax 3 wwmax 4 rwmax 2 wrmax 0
Load 2D firmware
Loaded Imaged id 33 of size 694c at address 18003000
Loaded Imaged id 35 of size 5bc at address 18003000
Execute 2D firmware
Applying PLL optimal settings
pll_ctrl2 = 0xb
pll_ctrl1 = 0x21
pll_test_mode = 0x24
pll_ctrl4 = 0x17f
End of initialization
End of initialization
End of initialization
2D Training failure
ERROR: Execution FW failed (err -5)
Program controller registers
twopass=0
PHY handshake timeout..., ddr_dsr2 = 0
total size 4 GB
Need to wait up to 1320 ms
ERROR: Found training error(s): 0x100
ERROR: Error: Waiting for D_INIT timeout.
ERROR: Writing DDR register(s) failed
ERROR: Programing DDRC error
ERROR: DDR init failed.
NOTICE: Incorrect DRAM0 size is defined in platform_def.h -5