LSDK21.08 LS1043AQDS SETUP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LSDK21.08 LS1043AQDS SETUP

ソリューションへジャンプ
560件の閲覧回数
SpringMelon
Contributor III

Hello, Wang. With your help, my board ls1043aqds has entered uboot. I use LSDK 21.08 for development, and the boot mode is TF-A. But my qspi flash is small, only 16MB, so I can't write itb directly to flash and start kernel and ramdisk from qspi.

I think the next priority is to burn the kernel and ramdisk into 16GB emmc, and then load the kernel from emmc. But I don't know if I have to use an external writer to burn emmc at the moment, and I don't know exactly what needs to be modified and compiled in the next work.

I really hope to get your help and look forward to your reply as soon as possible. thank you.

@yipingwang

タグ(1)
0 件の賞賛
返信
1 解決策
486件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You need to modify LS1043AQDS device tree according to your custom board.

In LSDK 21.08 build environment:

$ source setup.env

$ flex-builder -c linux -m ls1043aqds

Go to Linux Kernel source code components/linux/linux, please modify arch/arm64/boot/dts/freescale/fsl-ls1043a-qds.dts according to your custom board.

For example, please delete the following device node, if there is no IFC NOR flash on your custom board.

nor@0,0 {
compatible = "cfi-flash";
reg = <0x0 0x0 0x8000000>;
big-endian;
bank-width = <2>;
device-width = <1>;
};

 

Then rebuild Linux Kernel

$ flex-builder -c linux -m ls1043aqds

Regenerate itb image

$ flex-builder -i mkitb -r yocto:tiny

Get the image flexbuild_lsdk2108_github/build/images/lsdk2108_yocto_tiny_LS_arm64.itb

If you need to the bootpartition image, please regenerate it with the following command

$ flex-builder -i mkbootpartition -a arm64

元の投稿で解決策を見る

4 返答(返信)
524件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The emmc device is not removable, you could copy all your images to the USB device, then boot up the target board with image lsdk2108_yocto_tiny_LS_arm64.itb and deploy Ubuntu rootfs to emmc device in Linux on the target board.

For example under u-boot,

=> ext2load usb 0:1 0xa0000000 lsdk2108_yocto_tiny_LS_arm64.itb

=> bootm 0xa0000000#ls1043aqds

Under Linux on the target board, please run the following commands to deploy Kernel and Ubuntu rootfs to emmc device.

$ flex-installer -i pf -d /dev/mmcblk0

$ flex-installer -b boot_LS_arm64_lts_5.10.tgz -r rootfs_lsdk2108_ubuntu_main_arm64.tgz -d /dev/mmcblk0

Note:/dev/mmcblk0 is the emmc device name on the target board.

0 件の賞賛
返信
494件の閲覧回数
SpringMelon
Contributor III

Wang,Thank you very much for your technical reply, and I am honored to get your help in debugging this series of boards for the first time. I have made some progress following your suggestions, but it seems that the kernel is stuck and cannot continue. I have attached the log, and I hope to get your help on what I should do next so that I can successfully enter ramdisk.

@yipingwang 

0 件の賞賛
返信
487件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You need to modify LS1043AQDS device tree according to your custom board.

In LSDK 21.08 build environment:

$ source setup.env

$ flex-builder -c linux -m ls1043aqds

Go to Linux Kernel source code components/linux/linux, please modify arch/arm64/boot/dts/freescale/fsl-ls1043a-qds.dts according to your custom board.

For example, please delete the following device node, if there is no IFC NOR flash on your custom board.

nor@0,0 {
compatible = "cfi-flash";
reg = <0x0 0x0 0x8000000>;
big-endian;
bank-width = <2>;
device-width = <1>;
};

 

Then rebuild Linux Kernel

$ flex-builder -c linux -m ls1043aqds

Regenerate itb image

$ flex-builder -i mkitb -r yocto:tiny

Get the image flexbuild_lsdk2108_github/build/images/lsdk2108_yocto_tiny_LS_arm64.itb

If you need to the bootpartition image, please regenerate it with the following command

$ flex-builder -i mkbootpartition -a arm64

461件の閲覧回数
SpringMelon
Contributor III
Dear WANG,Thank you very much for your help, I can now enter the official ubuntu file system.
0 件の賞賛
返信