LSDK21.08 LS1043AQDS QSGMII LAN8814

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LSDK21.08 LS1043AQDS QSGMII LAN8814

595 Views
SpringMelon
Contributor III

Hello,Wang.In ls1043aqds, first I removed the ethernet@e4000 node (rgmii1), but the error was not found. However, several other qsgmii interfaces I defined also reported the same error. I'm depressed. Files related to the device tree are attached.

SpringMelon_0-1722238285949.png

@yipingwang 

Labels (1)
0 Kudos
Reply
7 Replies

566 Views
yipingwang
NXP TechSupport
NXP TechSupport

Discussing with the AE team.

0 Kudos
Reply

536 Views
SpringMelon
Contributor III
Hello,Wang.Could you tell me how to check this problem that fsl_dpa soc:fsl,dpaa:ethernet@0: of_find_device_by_node(ethernet@e0000) failed.
0 Kudos
Reply

535 Views
yipingwang
NXP TechSupport
NXP TechSupport

It seems that there is hardware problem that the QSGMII Ethernet ports cannot be probed in both u-boot and Linux Kernel at all.

0 Kudos
Reply

523 Views
SpringMelon
Contributor III
If I only need the kernel boot network port to be available, I don't need to modify it in uboot.
0 Kudos
Reply

504 Views
yipingwang
NXP TechSupport
NXP TechSupport

You can do MDIO tests on u-boot to examine the LAN8814 hardware first. Use mdio or mii commands on u-boot to read the PHY registers of LAN8814. If LAN8814 doesn't respond with reasonable values at MDIO transactions, it shall have some hardware issues.

=>mdio read  mdio@fc000 0x8 1

For all "F" result, it means there is problem with PHY hardware.

0 Kudos
Reply

501 Views
yipingwang
NXP TechSupport
NXP TechSupport

In your RCW configuration, you configured SRDS_PLL_REF_CLK_SEL_S1=0, please check whether the following is suitable for your target board.

SerDes 1, PLL1 : 0 - 100MHz for SGMII and PCIe

0 Kudos
Reply

547 Views
SpringMelon
Contributor III
How can I get it ?
0 Kudos
Reply