LS1043A-RGW secondary CPUs fail to come online

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1043A-RGW secondary CPUs fail to come online

2,733 次查看
andrewbarrow
Contributor I

I'm running LS1043A-RDB firmware I built with the LSDK, with hand-edited DTB file. The secondary CPUs fail to come online at boot. This happens with either 4.4 or 4.9 kernel.

I boot by U-Boot loading image and the DTB from SD card. 

NAND contents are the same as the RGW board comes with.

Am I missing a firmware image? Do I have a bad DTB? 

标签 (1)
0 项奖励
回复
9 回复数

2,035 次查看
andrewbarrow
Contributor I

Also is there a pre-compiled u-boot-sdboot.bin somewhere for the LS1043A-RGW (residential gateway)?

0 项奖励
回复

2,035 次查看
j_wallace
Contributor II

Hello Andrew.

Did you solve your issue?

B.R.

0 项奖励
回复

2,035 次查看
andrewbarrow
Contributor I

We did - we got a LS1043ARDB board and moved away from the ARGW board. Thanks.

0 项奖励
回复

2,035 次查看
j_wallace
Contributor II

Ok. Thanks for your feedback.

Best Regards.

0 项奖励
回复

2,035 次查看
andrewbarrow
Contributor I

I have LS1043A RGW (residential gateway) board and it has the newest u-boot image from the ASK loadable binaries, so I can't load the newer RDB u-boot onto it.

I am trying to load a Ubuntu image I made with LSDK and a DTB I hand-edited. Everything is working except I have no secondary CPUs coming up.

0 项奖励
回复

2,035 次查看
Pavel
NXP Employee
NXP Employee

Change u-boot on your LS1043ARDB board. Similar behavior happens if u-boot from previous version is used.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,035 次查看
andrewbarrow
Contributor I

Here are boot messages from RDB (boot freezes) and RGW (boots, no secondary CPUs)... differences highlighted:

Default LS1043ARDB LSDK file: fsl-ls1043a-rdb.dtb - boot freezes prior to CPUs coming online:

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.9.62 (root@saturn.ap.freescale.net) (gcc version 5.4.0 20160609 (Ubuntu/Linaro 5.4.0-6ubuntu1~16.04.4) ) #1 SMP PREEMPT Sat Dec 23 00:28:49 CST 2017
[ 0.000000] Boot CPU: AArch64 Processor [410fd034]
[ 0.000000] earlycon: uart8250 at MMIO 0x00000000021c0500 (options '')
[ 0.000000] bootconsole [uart8250] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] OF: reserved mem: initialized node qman-fqd, compatible id fsl,qman-fqd
[ 0.000000] OF: reserved mem: initialized node qman-pfdr, compatible id fsl,qman-pfdr
[ 0.000000] OF: reserved mem: initialized node usdpaa_mem, compatible id fsl,usdpaa-mem
[ 0.000000] OF: reserved mem: initialized node bman-fbpr, compatible id fsl,bman-fbpr
[ 0.000000] cma: Reserved 16 MiB at 0x00000000fb000000
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000000000000-0x00000000ffdfffff]
[ 0.000000] NUMA: Adding memblock [0x80000000 - 0xfbffffff] on node 0
[ 0.000000] NUMA: Adding memblock [0xff000000 - 0xff3fffff] on node 0
[ 0.000000] NUMA: Adding memblock [0xff800000 - 0xffdfffff] on node 0
[ 0.000000] NUMA: Initmem setup node 0 [mem 0x80000000-0xffdfffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xffdc74c0-0xffdc8c7f]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffdfffff]
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000fbffffff]
[ 0.000000] node 0: [mem 0x00000000ff000000-0x00000000ff3fffff]
[ 0.000000] node 0: [mem 0x00000000ff800000-0x00000000ffdfffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffdfffff]
[ 0.000000] WARNING: x1-x3 nonzero in violation of boot protocol:
[ 0.000000] x1: 0000000000000000
[ 0.000000] x2: 0000000000000000
[ 0.000000] x3: 0000000080080000
[ 0.000000] This indicates a broken bootloader or old kernel
[ 0.000000] percpu: Embedded 23 pages/cpu @ffff80007fd66000 s55000 r8192 d31016 u94208
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: enabling workaround for ARM erratum 845719
[ 0.000000] Built 1 zonelists in Node order, mobility grouping on. Total pages: 502280
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: root=/dev/mmcblk0p3 rw rootdelay=5 console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] Memory: 1709296K/2041856K available (12412K kernel code, 1054K rwdata, 4896K rodata, 1152K init, 978K bss, 316176K reserved, 16384K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] modules : 0xffff000000000000 - 0xffff000008000000 ( 128 MB)
[ 0.000000] vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000 (129022 GB)
[ 0.000000] .text : 0xffff000008080000 - 0xffff000008ca0000 ( 12416 KB)
[ 0.000000] .rodata : 0xffff000008ca0000 - 0xffff000009170000 ( 4928 KB)
[ 0.000000] .init : 0xffff000009170000 - 0xffff000009290000 ( 1152 KB)
[ 0.000000] .data : 0xffff000009290000 - 0xffff000009397a00 ( 1055 KB)
[ 0.000000] .bss : 0xffff000009397a00 - 0xffff00000948c5d4 ( 979 KB)
[ 0.000000] fixed : 0xffff7dfffe7fd000 - 0xffff7dfffec00000 ( 4108 KB)
[ 0.000000] PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000 ( 16 MB)
[ 0.000000] vmemmap : 0xffff7e0000000000 - 0xffff800000000000 ( 2048 GB maximum)
[ 0.000000] 0xffff7e0000000000 - 0xffff7e0001ff8000 ( 31 MB actual)
[ 0.000000] memory : 0xffff800000000000 - 0xffff80007fe00000 ( 2046 MB)
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 64.
[ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=4.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=64, nr_cpu_ids=4
[ 0.000000] NR_IRQS:64 nr_irqs:64 0
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] GIC CPU mask not found - kernel will fail to boot.
[ 0.000000] GIC CPU mask not found - kernel will fail to boot.
[ 0.000000] arm_arch_timer: Enabling workaround for FSL erratum A-008585
[ 0.000000] arm_arch_timer: Architected cp15 timer(s) running at 25.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c40939b5, max_idle_ns: 440795202646 ns
[ 0.000002] sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 4398046511100ns
[ 0.008460] Console: colour dummy device 80x25
[ 0.012951] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=100000)
[ 0.023350] pid_max: default: 32768 minimum: 301
[ 0.028054] Security Framework initialized
[ 0.032460] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes)
[ 0.040756] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes)
[ 0.048338] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.055071] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.062789] ASID allocator initialised with 65536 entries

--- boot freezes here ---

***

My .dtb, based on ls1043a-rgw DTB image for OpenWRT pre-compiled binary (boots, but secondary CPUs do not come online):

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.9.62 (root@saturn.ap.freescale.net) (gcc version 5.4.0 20160609 (Ubuntu/Linaro 5.4.0-6ubuntu1~16.04.4) ) #1 SMP PREEMPT Sat Dec 23 00:28:49 CST 2017
[ 0.000000] Boot CPU: AArch64 Processor [410fd034]
[ 0.000000] earlycon: uart8250 at MMIO 0x00000000021c0500 (options '')
[ 0.000000] bootconsole [uart8250] enabled
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] OF: reserved mem: initialized node qman-fqd, compatible id fsl,qman-fqd
[ 0.000000] OF: reserved mem: initialized node qman-pfdr, compatible id fsl,qman-pfdr
[ 0.000000] OF: reserved mem: initialized node bman-fbpr, compatible id fsl,bman-fbpr
[ 0.000000] cma: Reserved 16 MiB at 0x00000000fb000000
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000000000000-0x00000000ffdfffff]
[ 0.000000] NUMA: Adding memblock [0x80000000 - 0xfbffffff] on node 0
[ 0.000000] NUMA: Adding memblock [0xff800000 - 0xffdfffff] on node 0
[ 0.000000] NUMA: Initmem setup node 0 [mem 0x80000000-0xffdfffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xffdc8880-0xffdca03f]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffdfffff]
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000fbffffff]
[ 0.000000] node 0: [mem 0x00000000ff800000-0x00000000ffdfffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffdfffff]
[ 0.000000] WARNING: x1-x3 nonzero in violation of boot protocol:
[ 0.000000] x1: 0000000000000000
[ 0.000000] x2: 0000000000000000
[ 0.000000] x3: 0000000080080000
[ 0.000000] This indicates a broken bootloader or old kernel
[ 0.000000] percpu: Embedded 23 pages/cpu @ffff80007fd67000 s55000 r8192 d31016 u94208
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: enabling workaround for ARM erratum 845719
[ 0.000000] Built 1 zonelists in Node order, mobility grouping on. Total pages: 501256
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: root=/dev/mmcblk0p3 rw rootdelay=5 console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500
[ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.000000] Memory: 1967348K/2037760K available (12412K kernel code, 1054K rwdata, 4896K rodata, 1152K init, 978K bss, 54028K reserved, 16384K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] modules : 0xffff000000000000 - 0xffff000008000000 ( 128 MB)
[ 0.000000] vmalloc : 0xffff000008000000 - 0xffff7dffbfff0000 (129022 GB)
[ 0.000000] .text : 0xffff000008080000 - 0xffff000008ca0000 ( 12416 KB)
[ 0.000000] .rodata : 0xffff000008ca0000 - 0xffff000009170000 ( 4928 KB)
[ 0.000000] .init : 0xffff000009170000 - 0xffff000009290000 ( 1152 KB)
[ 0.000000] .data : 0xffff000009290000 - 0xffff000009397a00 ( 1055 KB)
[ 0.000000] .bss : 0xffff000009397a00 - 0xffff00000948c5d4 ( 979 KB)
[ 0.000000] fixed : 0xffff7dfffe7fd000 - 0xffff7dfffec00000 ( 4108 KB)
[ 0.000000] PCI I/O : 0xffff7dfffee00000 - 0xffff7dffffe00000 ( 16 MB)
[ 0.000000] vmemmap : 0xffff7e0000000000 - 0xffff800000000000 ( 2048 GB maximum)
[ 0.000000] 0xffff7e0000000000 - 0xffff7e0001ff8000 ( 31 MB actual)
[ 0.000000] memory : 0xffff800000000000 - 0xffff80007fe00000 ( 2046 MB)
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 64.
[ 0.000000] RCU restricting CPUs from NR_CPUS=64 to nr_cpu_ids=4.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=64, nr_cpu_ids=4
[ 0.000000] NR_IRQS:64 nr_irqs:64 0
[ 0.000000] GIC: Adjusting CPU interface base to 0x000000000142f000
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] arm_arch_timer: Enabling workaround for FSL erratum A-008585
[ 0.000000] arm_arch_timer: Architected cp15 timer(s) running at 25.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c40939b5, max_idle_ns: 440795202646 ns
[ 0.000002] sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 4398046511100ns
[ 0.008483] Console: colour dummy device 80x25
[ 0.012980] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=100000)
[ 0.023385] pid_max: default: 32768 minimum: 301
[ 0.028091] Security Framework initialized
[ 0.032501] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes)
[ 0.040802] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes)
[ 0.048388] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.055126] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes)
[ 0.062838] ASID allocator initialised with 65536 entries
[ 0.100790] EFI services will not be available.
[ 1.149902] CPU1: failed to come online
[ 1.153749] CPU1: failed in unknown state : 0x0
[ 2.210854] CPU2: failed to come online
[ 2.214701] CPU2: failed in unknown state : 0x0
[ 3.271804] CPU3: failed to come online
[ 3.275650] CPU3: failed in unknown state : 0x0
[ 3.280227] Brought up 1 CPUs

0 项奖励
回复

2,035 次查看
andrewbarrow
Contributor I

Here are some notable differences in the .dtb files that boot on one cpu only vs. fail to boot:

Default LS1043ARDB LSDK file: fsl-ls1043a-rdb.dtb - boot freezes prior to CPUs coming online:

interrupt-controller@1400000 {
   compatible = "arm,gic-400";
   #interrupt-cells = <0x3>;
   interrupt-controller;
   reg = <0x0 0x1401000 0x0 0x1000 0x0 0x1402000 0x0 0x2000 0x0 0x1404000 0x0 0x2000 0x0 0x1406000 0x0       0x2000>;
   interrupts = <0x1 0x9 0xf08>;
   linux,phandle = <0x1>;
   phandle = <0x1>;
};

firmware {

   optee {
   compatible = "linaro,optee-tz";
   method = "smc";
};

My .dtb, based on ls1043a-rgw DTB image for OpenWRT pre-compiled binary (boots, but secondary CPUs do not come online):

interrupt-controller@1400000 {
   compatible = "arm,gic-400";
   #interrupt-cells = <0x3>;
   interrupt-controller;
   reg = <0x0 0x1410000 0x0 0x10000 0x0 0x1420000 0x0 0x20000 0x0 0x1440000 0x0 0x20000 0x0 0x1460000 0x0    0x20000>;
   interrupts = <0x1 0x9 0xf08>;
   linux,phandle = <0x1>;
   phandle = <0x1>;
};

- note my dtb that boots on primary only has no OPTEE firmware 

So I'm thinking one of the following could be the problem:

1. the RGW board is missing the OPTEE firmware or PPA firmware (I haven't loaded any because I found no instructions for loading it to NAND on the RGW board). With no secure boot firmware, only CPU (needed for boot) comes up. 

2. the reg values for interrupt-controller are incorrect in the first case, giving "GIC CPU mask not found - kernel will fail to boot" error

3. I couldn't get booting from SD card to work on my RGW board, so I am booting from NAND with the following u-boot:

sdboot=setenv bootargs root=/dev/mmcblk0p3 rw rootdelay=5 console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500;mmcinfo;ext2load mmc 0:2 $loadaddr Image; ext2load mmc 0:2 a0000000 fsl-ls1043a-rdb.dtb; booti $loadaddr - a0000000

If the MMC image has e.g. OPTEE or PPA firmware present, I must be ignoring it as I only fetch kernel and dtb from MMC.

0 项奖励
回复

2,035 次查看
Pavel
NXP Employee
NXP Employee

It looks like that your DTB file is incorrect. Test your board using default version of the LS1043ARDB LSDK DTB file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复