LS1043A PCIe End point

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A PCIe End point

ソリューションへジャンプ
1,154件の閲覧回数
SrinivasP
Contributor II

Can we configure PCIe of  LS1043A as End point? If yes, is it with RCW register?

タグ(1)
0 件の賞賛
1 解決策
1,150件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LS1043A Reference Manual, 28.1 The PCI Express controller as implemented on the chip:

"NOTE
The EP mode is not supported in LS1043A; any references to that should be ignored."

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
1,142件の閲覧回数
SrinivasP
Contributor II

I want to get clarified on one more topic. As per PCIe spec and generation a specified transfer rate is mentioned (2. GT/s , 5 GT/s etc). Is this transfer rate fixed or can we configure any transfer rate below the maximum specified? 

0 件の賞賛
1,151件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LS1043A Reference Manual, 28.1 The PCI Express controller as implemented on the chip:

"NOTE
The EP mode is not supported in LS1043A; any references to that should be ignored."

0 件の賞賛
1,145件の閲覧回数
SrinivasP
Contributor II

Thank you

0 件の賞賛