Is there a typo in Errata A-010840 for the LS1021A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a typo in Errata A-010840 for the LS1021A

901件の閲覧回数
raymondhaas
Contributor I

I have been analyzing the Errata for the LS1021A processor, LS1021ACE, Rev. 10, 11/2018.  Specifically, I am looking at the workaround for A-010840. The workaround mentions a register bit DMR[SO].  I have looked in the reference manual, LS1021ARM Rev. 3 10/2018, and there is no bit called SO associated with this register. I was looking in section 30.2.1.2.

 

Is this a typo?  Am I misreading this?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

804件の閲覧回数
ufedor
NXP Employee
NXP Employee

I will provide response through the dedicated Technical Case.

0 件の賞賛
返信

804件の閲覧回数
raymondhaas
Contributor I

I am sorry. I posted this question minutes before I receive an answer from NXP support. I posted the question to NXP support on Feb 5th and didn’t receive an answer. I thought I would try the community site. Please disregard the question. Thank you

0 件の賞賛
返信

804件の閲覧回数
ufedor
NXP Employee
NXP Employee

The bit is shown as reserved in the RM.

The DMR[SO] is bit 3.

 

0 件の賞賛
返信