I'm currently in the process of porting the root file system onto the LS1028ardb board, which is booted via the composite firmware "firmware_ls1028ardb_uboot_sdboot.img."
rfs is generated via "bitbake ls-image-main" under the path:
build_ls1028ardb/tmp/deploy/images/ls1028ardb/ls-image-main-ls1028ardb-20231020060114.rootfs.tar.gz
I've come across a potential solution using the flex-installer tool with the following commands:
flex-installer -r <rootfs> -b <boot> -f <firmware> -d /dev/mmcblk0
However, I'm unable to locate the boot partition file for the LLDP SDK.
Here are the software details of the board:
ID=fsl-qoriq-distro
NAME="QorIQ SDK POC (Proof of Concept)"
VERSION="4.1.1 (langdale)"
VERSION_ID=4.1.1
PRETTY_NAME="QorIQ SDK POC (Proof of Concept) 4.1.1 (langdale)"
DISTRO_CODENAME="langdale"
root@ls1028ardb:~# uname -r
6.1.1+g29549c7073bf
Any assistance on this matter would be greatly appreciated.
regards,
Gourav Jain
can you pls share the ubuntu login credential of desktop image ??
Please use the command:
bitbake generate-boottgz
in order to generate the boot partition file .tgz , but you will need to start the environment once again.
regards
LFGP
you can use flex-installer as next:
$ flex-installer -r ls-image-main-<machine>.tar.gz -d /dev/mmcblk0 (or /dev/sdx)
but in your case :
$ flex-installer -r ls-image-desktop-<machine>.tar.gz -d /dev/mmcblk0 (or /dev/sdx)
please check the subject ""4.5.13 Upgrade the existing Layerscape LDP distro with Yocto bitbake on host""
also note the next when use bitbake:
$ bitbake ls-image-lite
$ bitbake ls-image-main # (if machine=ls1028ardb, should bitbake ls-image-desktop )
4.5.3 Build Layerscape LDP image using bitbake
Thanks,
It worked well.