DDR PHY: 1D training failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR PHY: 1D training failed

1,780件の閲覧回数
muaxi8
Contributor V

I have downloaded the Flash DDR Fip Binary to the address XSPI Nor 0x800000.

When I connected to the LX2080A (LX2160A Family) using CodeWarrior, I received the following error:

 DDR PHY: 1D training failed

muaxi8_0-1619851916224.png

What causes it and how can I fix it ?

My board‘’s uboot is now unable to get up, I guess that is the reason

Looking forward to reply

タグ(1)
0 件の賞賛
6 返答(返信)

1,690件の閲覧回数
eneyland
Contributor I

I am having this issue as well, would like to know the solution others had to clear it.

0 件の賞賛

1,770件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which board is in question?

How DDR SDRAM is implemented?

Which code is debugged?

What are the steps required to replicate the issue?

0 件の賞賛

1,755件の閲覧回数
muaxi8
Contributor V

Has been resolved

thanks!!

0 件の賞賛

1,386件の閲覧回数
deepanrajanbara
Contributor IV

Hi

Please let know , how the issue was resolved.

 

Thank you,

Deepanraj.A

0 件の賞賛

1,711件の閲覧回数
xmj
Contributor I

I have met the similar issue.  Could you post the solution?

 

Thanks in advance! 

0 件の賞賛

1,747件の閲覧回数
ufedor
NXP Employee
NXP Employee

Could you please explain the issue cause and the cure?

0 件の賞賛