Currently I have utilize all interface and pin available on LS1043 and I require to have an extra GPIO to identify my board version. By reviewing schematic of LS1043ARDB , I find that EVT0 to EVT4 pins are pull up with 4.7K register and not used at anywhere.
In technical reference manual of LS1043, Appendix C represent EPU register descriptions. Where EPU base address is 2000_0000h.
EVT0_ADDR -> 2000_0000 + (50h + (0 x 4h)) = 2000_0050 (EPEVTCR0)
EVT1_ADDR -> 2000_0000 + (50h + (1 x 4h)) = 2000_0054 (EPEVTCR1)
EVT2_ADDR -> 2000_0000 + (50h + (2 x 4h)) = 2000_0058 (EPEVTCR2)
EVT3_ADDR -> 2000_0000 + (50h + (3 x 4h)) = 2000_005C (EPEVTCR3)
EVT4_ADDR -> 2000_0000 + (50h + (4 x 4h)) = 2000_0060 (EPEVTCR4)
So if I configure 0th bit DIR as 0b then it will configure as input pin then I can read status of that pin from EPRSRSVn.
As per my understating if ENTn_B pin is configure with external pull-up then I will get value 1 from EPRSRSVn register.if ENTn_B pin configure with external pull-down then i will get value 0 from EPRSRSVn register.
Request you to confirm this, please let me know for any improvement or changes.
Regards,
Bhargav Jayswal
Solved! Go to Solution.
Hi @bhargavjayswal,
Apologies for the delayed response,
Yes, you can use this pin as an input in order to validate the pin state
Thank you @SebastianG ,
I have posted one more query today but it is not reflecting in NXP community. Title for the query is "LS1043A : EMMC GPT partitioning and boot process". Could you please help for this as well.
Hi @bhargavjayswal,
Yes, I will support in this query
Hi @bhargavjayswal,
This configuration seems good
Thanks for update.
Now based on above configuration, can we use this pin as an input gpio during u-boot to validate state of the pin whether is high or low?
Regards,
Bhargav Jayswal
Hi @bhargavjayswal,
Apologies for the delayed response,
Yes, you can use this pin as an input in order to validate the pin state