Hey, Guys,
I have started VPP on my ls1046ardb board, and did the test cases successfully from lsdk user guide.
Now, I wanna investigate more about performance, so I checked the buffer usage on VPP, but the statistics are very confusing, though the function is all right, packets forwarding right:
vpp# show buffers
Pool Name Index NUMA Size Data Size Total Avail Cached Used
default-numa-0 0 0 2496 2048 16000 15968 34 42949672
vpp# show buffers
Pool Name Index NUMA Size Data Size Total Avail Cached Used
default-numa-0 0 0 2496 2048 8000 8000 0 0
For comparison, I tested the same case on the X86 platform<VPP 21.01>, I can see the "show buffer" works well:
vpp# show buffers
Pool Name Index NUMA Size Data Size Total Avail Cached Used
default-numa-0 0 0 2304 2048 16808 16296 152 360
vpp# show buffers
Pool Name Index NUMA Size Data Size Total Avail Cached Used
default-numa-0 0 0 2304 2048 16808 16296 154 358
So there are two questions:
1, Is the VPP repo in lsdk21.08 the same as https://github.com/nxp-qoriq/vpp/releases/tag/21.08-LSDK and modified from the origin repo https://github.com/FDio/vpp/releases/tag/v21.01
2. do you guys have any idea about this issue, any relative modifications about buffer pool management you have done?
Any replies will be helpful.
Thanks
Hello,
Please refer to NXP latest LSDK release for Layerscape https://www.nxp.com.cn/docs/en/user-guide/LLDPUG_RevL6.1.22_2.0.0.pdf
VPP version is as the following.
VPP v23.02 build with DPDK 22.11.
LLDPUG is based on Yocto, LSDK is based on flex-builder.
LLDPUG is newer than LSDK.
LLDPUG will replace LSDK in feature.
Regards
hey Bio_TICFSL,
Thanks for the advice, I have booted the latest LSDK release image, and the buffers seem to show right.
But there is another issue, I'm doing the forwarding test by VPP.
Topology:
PC<port0> <-----> <fm1-mac3> ls1046ardb <fm1-mac4> <------> PC<port1>
Result:
PC Statistics:
FM Port:
VPP:
According to the result, you can see the FM port got all the packets, but VPP dpdk-input rx lost about 1.5M packets, and I can't see anything wrong in vpp.
Do you have any idea about where to check the lost packets?
Best Regards
Skyler.
Hey, Bio_TICFSL,
A few updates:
1) the lost packets is located, all in port_discard_frame </sys/devices/platform/soc/1a00000.fman/1a8a000.port/statistics>
2) I tested on rgmii port with trex<100% bandwidth>, when frame size is 1518, no frame discard, but once frame size is 64, many discards.
As you know, a smaller frame size means more frames. so maybe the frame queue is up to threshold?
I'm still working on it.
Any suggestion will be helpful.
Best Regards,
Skyler.