Compiling 88W9098 PCIe for LS1012A Dev Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compiling 88W9098 PCIe for LS1012A Dev Board

1,009 Views
cdubs14
Contributor II

Hi,

I’m using the Type 1XL from Murata which uses the 88W9098 NXP chip and connects to the host via PCIe. I’ve plugged this board into a FRWY LS1012A development board running Layerscape. I’ve tried following the attached instructions from NXP for compiling the driver, but run into issues with the ‘make build’ command. I know I’m missing something with the Linux kernel but can’t figure out what, does anyone know how to resolve this to get the WiFi chip working?

Tags (3)
0 Kudos
Reply
3 Replies

792 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "11.1 Connectivity for Bluetooth wireless technology and Wi-Fi" in i.MX_Linux_Users_Guide.pdf

0 Kudos
Reply

876 Views
kenli
NXP Employee
NXP Employee

question is not clear,u mean how to build the driver of 88w?

Best regards
0 Kudos
Reply

862 Views
cdubs14
Contributor II

Yep, just trying to compile the 88W9098 driver. I have the driver’s ‘make’ file, but I can’t figure out how to configure my Linux kernel to allow the ‘make build’ command execute successfully.

 

I’ve read online that I need to download and ‘setup’ the kernel, but I’m confused as to why that’s a step if I’m already running on the kernel version I’d like to use to building this driver. 

0 Kudos
Reply