Clarification on instructions how to programm u-boot into NOR flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clarification on instructions how to programm u-boot into NOR flash

ソリューションへジャンプ
5,855件の閲覧回数
reinhardtartler
Contributor I

Board: LS1021A-TWR

We are experiencing trouble with following the instructions from the SDK Documentation at Freescale Technical Information Center

The instructions in "Programming a new New U-Boot" do not result in a working u-boot in Bank 1.

However, posts in this forum indicate that the correct address to program is 0x63f80000 instead:

TWR-LS1021A : U-boot console prompt not shown in LPUART mode

How do I recover from a failed u-boot flash on the LS1021A?

We could confirm that flashing u-boot to that address does result in a working u-boot in Bank 1. Curiously, there is no disagreement on the location of the RCW (0x64000000), but only u-boot: 0x64100000 (wrong) vs 0x63f80000. Also, the 2nd discussion forum claims that the correct location for u-boot in bank 0 was 0x67f80000. This is also inconsistent to the memory map given for the Flash Bank Usage: Flash Bank Usage.

Please clarify the instructions in the SDK documentation, in particular the Flash Bank memory map.

Thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
5,526件の閲覧回数
Pavel
NXP Employee
NXP Employee

Correct information about addresses for the NOR Flash using on the LS1021a board is available in documentation in SDK iso file.

Attached file contains pages from this documentation.

0x63f80000 0x63ffffff bank4 u-boot image 512 K

0x67f80000 0x67ffffff bank0 u-boot image 512 K

Freescale Technical Information Center will be corrected.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,527件の閲覧回数
Pavel
NXP Employee
NXP Employee

Correct information about addresses for the NOR Flash using on the LS1021a board is available in documentation in SDK iso file.

Attached file contains pages from this documentation.

0x63f80000 0x63ffffff bank4 u-boot image 512 K

0x67f80000 0x67ffffff bank0 u-boot image 512 K

Freescale Technical Information Center will be corrected.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
5,526件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello,

I have tried on my board with "63f80000" for bank 1 u-boot on my board, and it works fine.

Regards

0 件の賞賛
返信