Hi There,
I want to check how to use the USB controller of LS1046A.
There is a difference between the contents of the reference board and the application note.
Please tell me the correct unused processing the following conditions.
[Conditions]
・USB1 works with USB2.0.
・USB2 / 3 is unused.
【Check】
1.Does USB [2/3] _VBUS need a 5V power supply?
2.Is the USB [2/3] _ID 1kΩ connection correct?
3.Does USB [1] _RESREF require 200Ω?
4.Does USB [2/3] _RESREF require 200Ω?
Best regards
- satoshi
已解决! 转到解答。