PHY handshake timeout..., ddr_dsr2 = 0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PHY handshake timeout..., ddr_dsr2 = 0

11,108 Views
muaxi8
Contributor V

platform: LX2080a

ddr4:  MT40A512M16JY ,8Gb, x16 width

I program the bl2_flexspi_nor.pbl,  fip_uboot.bin, fip_ddr_all.bin  on the specific address。

The following print appears when  my board is power on。What causes DDR PHY to fail ? 

i  have Defined macro “CONFIG_STATIC_DDR” in plat/nxp/<SOC>/<BOARD>/plafform_def.h to enable discrete DDR timings.

NOTICE:  BL2: v2.3():v2.3-LSDK-20.12-dirty
NOTICE:  BL2: Built : 18:47:53, May  7 2021
twopass=0
PHY handshake timeout..., ddr_dsr2 = 0
ERROR:   Found training error(s): 0x100
ERROR:   Error: Waiting for D_INIT timeout.
ERROR:   Writing DDR register(s) failed
ERROR:   Programing DDRC error
ERROR:   DDR init failed.
NOTICE:  Incorrect DRAM0 size is defined in platform_def.h

 

0 Kudos
Reply
17 Replies

11,057 Views
muaxi8
Contributor V
  1. 补充:
    芯片型号:LX2080XE72232B

  2. ddr4: MT40A512M16JY-083EIT
0 Kudos
Reply

11,014 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached QCVS DDRv user manual. 

Please configure "Properties" panel according to your DDR data sheet, then generate the initial DDR controller configuration parameter. Then you need to connect DDRv tool to your target board to optimize and validate these DDR configuration parameters.

0 Kudos
Reply

11,015 Views
muaxi8
Contributor V

yes, i connected DDRv tool to my target board,and "start validation", but it is Execution failed and will not proceed。I tried  several times but  still failed.

muaxi8_0-1621588047058.png

 

0 Kudos
Reply

10,968 Views
yipingwang
NXP TechSupport
NXP TechSupport

Would you please open CCS(CodeWarrior Connection Server) console, type "log v" command, then connect to the target board again? The low level CCS log will be printed. Please capture the CCS log and attach it to this thread.

0 Kudos
Reply

10,951 Views
muaxi8
Contributor V

The attachment is the log, but the previous contents seem to have been flushed out..

There was a mistake at the beginning:

muaxi8_0-1621911773201.png

 

0 Kudos
Reply

10,942 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "DDR Bring up issue"(page 2)  and "DDR Bring up HW checklist" (page 4)  sections in the attached document.

0 Kudos
Reply

10,920 Views
xmj
Contributor I

Hi yipingwang, 

Is this documentation also for LX2160A? 

Thanks

0 Kudos
Reply

10,885 Views
yipingwang
NXP TechSupport
NXP TechSupport

This document is also for LX2160A.

0 Kudos
Reply

10,971 Views
yipingwang
NXP TechSupport
NXP TechSupport

Would you please provide Error capture registers values?

0 Kudos
Reply

10,953 Views
muaxi8
Contributor V

 this is the  Error capture registers values...there valuse are all 0x0

muaxi8_0-1621912246038.png

 

muaxi8_1-1621912272509.png

 

muaxi8_2-1621912320803.png

 

muaxi8_3-1621912337942.png

 

 

0 Kudos
Reply

11,089 Views
yipingwang
NXP TechSupport
NXP TechSupport

You need to modify "const struct ddr_cfg_regs static_1600" in atf/plat/nxp/<SOC>/<BOARD>/ddr_init.c according to the DDR on your target board.

You could use QCVS DDRv tool to assist you to calculate DDR controller configuration parameters and optimize them.

0 Kudos
Reply

11,080 Views
muaxi8
Contributor V

 

AS the following figure。there is a Lead-in paramter , don't know how to fill in this parameter, How do I get this parameter?

muaxi8_0-1620976555169.png

Thank you for your reply

0 Kudos
Reply

11,059 Views
yipingwang
NXP TechSupport
NXP TechSupport

No need to fill this parameter.

0 Kudos
Reply

11,027 Views
muaxi8
Contributor V

muaxi8_0-1621501163204.png

Does the DQ mapping need to be configured? my dram type is discrete...

0 Kudos
Reply

11,032 Views
muaxi8
Contributor V

help me please

0 Kudos
Reply

11,051 Views
muaxi8
Contributor V

  I configured the above values based on the hardware's CLK To DQS parameters, and then generated the code in CodeWarrior, i Copy the static_1600 to my source code

 

 

const struct ddr_cfg_regs static_1600 = {
        .cs[0].config = 0x80010412,
        .cs[0].bnds = 0xFF,
        .sdram_cfg[0] = 0x65240000,
        .sdram_cfg[1] = 0x00401030,
        .timing_cfg[0] = 0x8055000C,
        .timing_cfg[1] = 0x0A0E0C42,
        .timing_cfg[2] = 0x0048D11C,
        .timing_cfg[3] = 0x11511000,
        .timing_cfg[4] = 0x01,
        .timing_cfg[5] = 0x05401400,
        .timing_cfg[7] = 0x23340000,
        .timing_cfg[8] = 0x07116600,
        .sdram_mode[0] = 0x01010234,
        .sdram_mode[9] = 0x0701,
        .sdram_mode[8] = 0x00,
        .sdram_mode[2] = 0x00,
        .sdram_mode[10] = 0x04000000,
        .sdram_mode[11] = 0x00,
        .sdram_mode[4] = 0x00,
        .sdram_mode[12] = 0x00,
        .sdram_mode[13] = 0x00,
        .sdram_mode[6] = 0x00,
        .sdram_mode[14] = 0x00,
        .sdram_mode[15] = 0x00,
        .interval = 0x18600618,
        .zq_cntl = 0x8A090705,
        .wrlvl_cntl[0] = 0x00,
        .wrlvl_cntl[1] = 0x00,
        .wrlvl_cntl[2] = 0x00,
        .debug[28] = 0x01080F70
};

 

 

 

After compiling with the flex-builder -c atf -m lx2160ardb_rev2 -b xspi command, bl2_flexspi_nor.pbl and fip_uboot.bin,programmed it to the  Flash, but it still prompts the 2D Training .(I turned on the Debug switch).Debugging several days, all the time not to the main point

 

 

muaxi8_0-1621335185653.png

 The following is the log information, looking forward to your reply...

 

NOTICE:  BL2: v2.3():v2.3-LSDK-20.12-dirty
NOTICE:  BL2: Built : 16:15:55, May 18 2021
platform clock 800000000
DDR PLL1 1600000000
DDR PLL2 1600000000
frequency = 800MHz
Vref_phy = 75 percent
Initializing input adv data structure
mr[0] = 0x234
mr[1] = 0x101
mr[2] = 0x0
mr[3] = 0x0
mr[4] = 0x0
mr[5] = 0x0
mr[6] = 0x0
input->cs_d0 = 0x3
input->cs_d1 = 0x0
input->mirror = 0x0
PHY ODT impedance = 48 ohm
PHY DQ driver impedance = 28 ohm
PHY Addr driver impedance = 30 ohm
odt[0] = 0x1
odt[1] = 0x0
odt[2] = 0x0
odt[3] = 0x0
Initializing message block
msg_blk->dram_type = 0x2
msg_blk->sequence_ctrl = 0x31f
msg_blk->phy_cfg = 0x0
msg_blk->x16present = 0x3
msg_blk->dramfreq = 0x640
msg_blk->pll_bypass_en = 0x0
msg_blk->dfi_freq_ratio = 0x2
msg_blk->phy_odt_impedance = 0x0
msg_blk->phy_drv_impedance = 0x0
msg_blk->bpznres_val = 0x0
msg_blk->enabled_dqs = 0x48
msg_blk->acsm_odt_ctrl0 = 0x1
msg_blk->acsm_odt_ctrl1 = 0x0
msg_blk->acsm_odt_ctrl2 = 0x0
msg_blk->acsm_odt_ctrl3 = 0x0
rx2d_train_opt 0, tx2d_train_opt 0
Initialize PHY 0 config
pll_ctrl2 = 0xb
SOC_SI_REV = 2
dll_lck_param = 0x212
dll_gain_ctl = 0x61
acx4_anib_Dis 0x0
Load 1D firmware
Loaded Imaged id 32 of size 6bd0 at address 18003000
Loaded Imaged id 34 of size 6d0 at address 18003000
Execute firmware
Applying PLL optimal settings
pll_ctrl2 = 0xb
pll_ctrl1 = 0x21
pll_test_mode = 0x24
pll_ctrl4 = 0x17f
End of fine write leveling
1D Training completed
Error - Invalid cs_in_use value 0
CDD rrmax 3 wwmax 4 rwmax 2 wrmax 0
Load 2D firmware
Loaded Imaged id 33 of size 694c at address 18003000
Loaded Imaged id 35 of size 5bc at address 18003000
Execute 2D firmware
Applying PLL optimal settings
pll_ctrl2 = 0xb
pll_ctrl1 = 0x21
pll_test_mode = 0x24
pll_ctrl4 = 0x17f
End of initialization
End of initialization
End of initialization
2D Training failure
ERROR:   Execution FW failed (err -5)
Program controller registers
twopass=0
PHY handshake timeout..., ddr_dsr2 = 0
total size 4 GB
Need to wait up to 1320 ms
ERROR:   Found training error(s): 0x100
ERROR:   Error: Waiting for D_INIT timeout.
ERROR:   Writing DDR register(s) failed
ERROR:   Programing DDRC error
ERROR:   DDR init failed.
NOTICE:  Incorrect DRAM0 size is defined in platform_def.h -5

 

 

 

 

 

 

 

0 Kudos
Reply

11,019 Views
xmj
Contributor I

I am working on the same issue......

0 Kudos
Reply