LPC54018J4MET, hardfault after bss_init when using XIP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54018J4MET, hardfault after bss_init when using XIP

766 次查看
ronwal
Contributor III

Hello

I created a new baremetal project based on the SDK_2.14_LPC54018J4M for my custom board. Without own code!

Running the project as "plain load image" is working but when I set it up as "XIP" i´ll face the following hardfault after the bss_init section.

  • <signal handler called>() at 0xfffffff9"
  • HardFault_Handler() at semihost_hardfault.c:53 0x1000193a
  • UFSR INVSTATE

ronwal_0-1699367492604.png

Just for information:

Loading the same project on a LPC54S018 EVK works just fine.

 

Regards

Ron

 

 

0 项奖励
回复
3 回复数

746 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ronwal 

How about import a SDK demo with XIP?

 

BR

Alice

0 项奖励
回复

740 次查看
ronwal
Contributor III

@Alice_Yang 

I tried that, but it´ll show the same hardfault!

标记 (1)
0 项奖励
回复

702 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ronwal 

 

Take video show your detail steps.

 

BR

Alice

0 项奖励
回复