Gray folders

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,016件の閲覧回数
mariob
Contributor III

Hi,

I try to implement a Vcom Port (CDC) on an PN7462. I need to use USBD_ROMStack.

But this folder is greyed out and strike through. I searched a lot, but wasn't able to find the meanig

of the grey folders and files.

Gray folders.jpg

Im sure this is no big issue.

Best Regards 

Mario

ラベル(1)
0 件の賞賛
返信
1 解決策
4 返答(返信)
5,444件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Are these folder perhaps marked as excluded from the build? Right click on them in the Project Explorer view and check the settings in the "Resouce Configurations" entry.

I also note that your project is using linked references. Make sure these folders actually exist in the linked location.

Regards,

LPCXpresso Support

0 件の賞賛
返信
5,444件の閲覧回数
mariob
Contributor III

Hi,

thank you for your reply. No this files are not excluded from the build. The folders are 

also existing. It's from the PN7462 examples witch you can download from here:

PN746X_736X_SERIES|NXP 

Best Regards

Mario

0 件の賞賛
返信
5,445件の閲覧回数
converse
Senior Contributor V
5,444件の閲覧回数
mariob
Contributor III

Hi Con Verse,

thank you very much. This solved my problem.

Best Regards 

Mario

0 件の賞賛
返信