Unable to Toggle the Port 0 pin 15 for Cortex M3 1788 Microcontroller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to Toggle the Port 0 pin 15 for Cortex M3 1788 Microcontroller

858 次查看
ankitvats
Contributor I

Hi, 

I write the Firmware in which I am Toggling  the  Port 0 Pin 15.
Toggling of  Pin on LPC1788 development kit is working But on Custom Board its not working.
On Custom Board , Port 0 Pin 16, 17, 18 I able to control.
According to Schematics of  Board , Pin 15 is connected to AND Gate.

So, can you Guide us.

0 项奖励
回复
3 回复数

845 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ankitvats 

 

Could you please show your schematic about "Pin 15 is connected to AND Gate."?

 

BR

Alice

0 项奖励
回复

837 次查看
ankitvats
Contributor I

Hi,

 MIC_RST_PCIe is P015 pin.

MicroController_Pins.JPG

AND_POWERSupply.JPG

 

 

0 项奖励
回复

808 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ankitvats 

How about use a simple project, only includes toggle P0_15 code? And measure on directly on P0_15 pin.

 

BR

Alice

0 项奖励
回复