LPC824 I2C sample code build error"Linker CRP Enabled, but no CRP_WORD provided within application."

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC824 I2C sample code build error"Linker CRP Enabled, but no CRP_WORD provided within application."

577 Views
Leo_Li
Contributor I

Hi, I recently want to learn how to use LPC824(HVQFN33)'s I2C0 (Pin 8, Pin 9) as a SLAVE in an I2C device. I looked into the recommended learning resources in the forum and wanted to try out the functionality.(https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC824-as-I2C-Sensor-Hub/td-p/730664)

However, during the DEBUG Build, I encountered the error message "Linker CRP Enabled, but no CRP_WORD provided within application." There is no indication of the location, and I'm unsure how to proceed. Has anyone else encountered a similar issue?

Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

556 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The CRP is invoked by programming a specific pattern in flash location at 0x0000 02FC for LPC82x.

 For detailed inf, pls refer to section 25.5.3 Code Read Protection (CRP).

xiangjun_rong_0-1703653371718.png

 

From software perspective, you can define the CRP in the startup_lpc804.c

#include <NXP/crp.h>

__CRP const unsigned int CRP_WORD = CRP_NO_CRP ;

 ////////////////////////////////////////////////////////

 

 

 

The CRP_NO_CRP is defined in the crp.h

#ifndef _CRP_H_INCLUDED_

#define _CRP_H_INCLUDED_

 

// A macro for placing data into the Code Read Protect (CRP) section,

// which is then located at the correct address for the selected MCU

// by the automatically generated linker script. The CRP section should

// contain a single 32-bit value which is the CRP value. See appropriate

// documentation for the MCU to determine CRP values.

//

// This feature is only available for NXP MCU targets with the Code Read

// Protect Feature

//

// Example:

// __CRP const uint32_t CRP_WORD = CRP_NO_CRP ;

//

#define __CRP __attribute__ ((used,section(".crp")))

 

#define CRP_NO_CRP 0xFFFFFFFF

 

// Disables UART and USB In System Programming (reads and writes)

// Leaves SWD debugging, with reads and writes, enabled

#define CRP_NO_ISP 0x4E697370

 

// Disables SWD debugging & JTAG, leaves ISP with with reads and writes enabled

// You will need UART connectivity and FlashMagic (flashmagictool.com) to reverse

// this. Don't even try this without these tools; most likely the SWD flash

// programming will not even complete.

// Allows reads and writes only to RAM above 0x10000300 and flash other than

// sector 0 (the first 4 kB). Full erase also allowed- again only through UART

// and FlashMagic (NO JTAG/SWD)

#define CRP_CRP1 0x12345678

 

// Disables SWD debugging & JTAG, leaves UART ISP with with only full erase

// enabled. You must have UART access and FlashMagic before setting this

// option.

// Don't even try this without these tools; most likely the SWD flash

// programming will not even complete.

#define CRP_CRP2 0x87654321

 

/************************************************************/

/**** DANGER CRP3 WILL LOCK PART TO ALL READS and WRITES ****/

#define CRP_CRP3_CONSUME_PART 0x43218765

/************************************************************/

 

xiangjun_rong_1-1703653863609.png

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply