Hello !
Do I understand right and MCU can be totally crystalless ? And supports whole declared temperature range ?
PLL0 can use FRO_12MHz and generate 100 or 150 Mhz clocks without any problems.
SPi and I2C can use FRO_12Mhz for clocking ( SPI speed can be 10Mhz ?).
RTC can own FRO32KHz oscillator but it may be not so precise for keep calendar time.
Is this so ? How to calculate possible drift while 1 week ?
What can be problems if no any crystals is not in use ?
Regards,
Eugene
已解决! 转到解答。
Hi Eugene,
LPC55S69 can be used without external crystal. However, you will not be able to use USB High-Speed without it and RTC will not be as accurate as using external crystal.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Eugene,
LPC55S69 can be used without external crystal. However, you will not be able to use USB High-Speed without it and RTC will not be as accurate as using external crystal.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------