LPC54616J512BD208 ADC conversion reading drooping after 5-8 minutes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54616J512BD208 ADC conversion reading drooping after 5-8 minutes

1,090 次查看
Heiser
Contributor I

Hello,

We are seeing an issue on our microcontroller where after around 5-8 minutes the ADC reading is dropping ~100 ADC bits on 3 ADC channels being converted, when the input being sampled on the channel's is not fluctuating.

We are using the conversion sequence A to get the ADC results from the 3 channels every 1ms. At the end of the sequence interrupt, the software trigger is being used to loop back through and get the conversions again.

The ADC reference voltage is tied to the 3.3V supply - this voltage is also not changing.

I have attached the ADC config routine and sequence handler plus the raw ADC readings captured over an hour.

Any help would be greatly appreciated.

 

标签 (1)
0 项奖励
回复
3 回复数

1,057 次查看
Heiser
Contributor I

Hi @Alexis_A ,

I think we have found the issue - one of the other ADC input channels had a negative voltage that would slowly drift down from 0V to ~-0.7V. When the channel measured around -0.3V this would then affect the ADC readings. It was repeatable with an external power supply.

Best Regards,

Heiser

1,052 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Heiser,

I'm glad that you could find the issue.

Only as a suggestion, to ensure the correct functionality of the MCU, the tolerance for negative voltage is limited to -0.5V.

Best Regards,

Alexis Andalon

0 项奖励
回复

1,064 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Heiser,

Looking at the configurations this looks good but this behavior seems strange. I have some questions about this:

Could you let me know which SDK version are you using?

Is there any event that could trigger this behavior in your application? Some signal that could introduce noise to the ADC capture?

Is this present using any channel?

As reference, in the following document there's some recommendations to improve the ADC measurement.

Best Regards

Alexis Andalon

0 项奖励
回复