Hello all,
I have just made a new PCB with an LPC1549 - 48 on it.
Absolute minimum parts,
USB connection, P2-12, P2-13
Pull-up’s for:
Reset,
ISP-0, P0-4
ISP-1 P0-16
I2C, P0-23, P0-22
CAN-TXD P0-13
CAN-RXD P0-18
Serial P0-15, P0-14
12 Mhz Crystal
And 2 LED’s
My problem is it does NOT show up as a USB Device, for programming,
It is not even coming up as a BAD Device !!
ISP-0 Low & ISP-1 Hi, and a negative going pulse on reset,
with reset low, my board takes about 4mA
When Hi around 9mA
I have made several other PCB designs, with USB enabled chips,
And they have worked OK.
Is there something I am missing, I have searched the data sheet for … you must …
or other Gothcers !!!
I can not see anything in the Espresso board that is relay different,
Other than I am using a 48 pin part not 64 pin part.
I am confident most of the board works, because I can enter serial ISP, and send “?”
and get
“Synchronized” back !!
But of course, using my work PC , I cannot install Flash Magic, or Bin2Hex
Only ‘APPROVED’ software is permitted
Any one has any suggestions,
I would appreciate it,
Cheers
Ceri
This is my version:
And the copper:
with CAN circuitry as well,
There is a 100R resistor in C16 slot, pulling RTX-IN low (as in data sheet, if not used)
I am still not able to get USB IAP to work.
I notice though two things, on your schematic:
Boot 0 and Boot 1 connected, which I believe means you can only go into serial boot (I need USB Programming)
and those are not the CAN pins for 48 pin device ?
You need of course to set the correct ISP mode.
You can run CAN on any pins
I use:
// CAN signal muxing LQFP48
Chip_SWM_MovablePortPinAssign(SWM_CAN_TD1_O , 0, 27); // P0.27 CAN TxD
Chip_SWM_MovablePortPinAssign(SWM_CAN_RD1_I, 0, 28); // P0.28 CAN RxD