Ethernet RMII CRS/DV signal is missing on the 100-pin version of LPC54606

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet RMII CRS/DV signal is missing on the 100-pin version of LPC54606

1,636 次查看
post
Contributor I

Hello,

an input for the Ethernet RMII Carrier Sense/Data Valid signal is missing on the 100-pin package version of LPC54606. Does somebody know if i can use the ENET_RX_DV (Ethernet receive data valid) input instead?

Thanks,

Rouslan

标签 (1)
0 项奖励
回复
2 回复数

1,321 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Rouslan Timofeev,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Does somebody knows if I can use the ENET_RX_DV (Ethernet receive data valid) input instead?
-- Yes, you can, and you can refer to the SCH of LPC54608 board for details.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,321 次查看
post
Contributor I

Thank you!

0 项奖励
回复