Ethernet RMII CRS/DV signal is missing on the 100-pin version of LPC54606

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet RMII CRS/DV signal is missing on the 100-pin version of LPC54606

2,790件の閲覧回数
post
Contributor I

Hello,

an input for the Ethernet RMII Carrier Sense/Data Valid signal is missing on the 100-pin package version of LPC54606. Does somebody know if i can use the ENET_RX_DV (Ethernet receive data valid) input instead?

Thanks,

Rouslan

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,475件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Rouslan Timofeev,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Does somebody knows if I can use the ENET_RX_DV (Ethernet receive data valid) input instead?
-- Yes, you can, and you can refer to the SCH of LPC54608 board for details.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,475件の閲覧回数
post
Contributor I

Thank you!

0 件の賞賛
返信