Some processors in LPC family have EMC, which enable customer to connect external parallel SRAM, NOR flash, SDRAM, there is application which saves code in serial flash for example SPI flash or IIC flash, copy the code to SDRAM and run code in SDRAM.
This is a simple code to demo how to run the code in SDRAM, the Code is developed under the SDRAM example code with SDK package, which initialize SDRAM and write data to SDRAM, read the data from SDRAM, compare whether the writing data and reading data are the same. A simple function void LED_Toggle(void) is used to toggle a LED, the API function is copied to SDRAM with the function void mem2mem(uint16_t *sourceAdd,uint16_t *destinationAdd,uint16_t length), after the function is called, an function pointer is defined and jump to the function pointer.
BTW, if user would like to run code in SDRAM, the MPU module for the Cortex-M4 has to be initialized, which enable the code in SDRAM to be fetched and executed.
The Demo code is developed under MCUXpresso ver10.3.1 and LPCXpresso546xx board(OM40003).
after you Run code, the LED2 can toggle on LPCXpresso546xx board..
I list the main code here. All the project is attached.
void mem2mem(uint16_t *sourceAdd,uint16_t *destinationAdd,uint16_t length)
{
sourceAdd = (uint16_t *)((uint32_t)sourceAdd & (0xFFFFFFFE));
destinationAdd=(uint16_t *)((uint32_t)destinationAdd & 0xFFFFFFFE);
for(uint16_t i=0; i<length; i++)
{
destinationAdd[i]=sourceAdd[i];
}
__DSB();
__ISB();
}
#define SDRAM_BASE_ADDR_CODE 0xa0000001
typedef void (*functionPointer)(void);
//The PC value must be an odd value although the code address is an even //value
void runCodeInSDRAM(void)
{
((functionPointer)SDRAM_BASE_ADDR_CODE)();
}
void LED_Toggle(void)
{
while(1)
{
delay_1();
GPIO->NOT[3]|=1<<3;
}
}
void MPU_Init(void)
{
//disable MPU
MPU->CTRL=0x00;
//Region0: default region 0
MPU->RBAR=0x00000010;
MPU->RASR=0x1004003f;
//Region 1:
//set up flash, ROM, SRAM ... as region 1
//# 0x00000000 - 0x3FFFFFFF
MPU->RBAR=0x00000011;
MPU->RASR=0x0306E23b;
//Region 2:
//set up peripheral device
//# 0x40000000 - 0x400FFFFF
MPU->RBAR=0x40000012;
MPU->RASR=0x13050033;
//Region 3:
//set up chip select and device
//# 0x80000000 - 0x9000FFFF
MPU->RBAR=0x80000013;
MPU->RASR=0x1305001f;
//Region 4:
//set up SDRAM
//# # 0xA0000000 - 0xA0FFFFFF
MPU->RBAR=0xa0000014;
MPU->RASR=0x0307002f;
//Region 5:
//set up Cortex-M4 Private Peripheral Bus
//# 0xE0000000 - 0xE00FFFFF
MPU->RBAR=0xe0000015;
MPU->RASR=0x13040027;
//Region 6:
//set up Not used
//# 0xE0000000 - 0xE00FFFFF
MPU->RBAR=0xe0000016;
MPU->RASR=0x00000000;
//Region 7:
//set up stack
//#
MPU->RBAR=0x1000E017;
MPU->RASR=0x10060009;
//enable MPU
MPU->CTRL=0x01;
}
int main(void)
{
uint32_t index;
uint32_t *sdram = (uint32_t *)SDRAM_BASE_ADDR; /* SDRAM start address. */
/* Hardware Initialization */
CLOCK_EnableClock(kCLOCK_InputMux);
/* attach 12 MHz clock to FLEXCOMM0 (debug console) */
CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);
BOARD_InitPins();
BOARD_BootClockFROHF96M();
BOARD_InitDebugConsole();
LEDInit();
//LED_Toggle();
BOARD_InitSDRAM();
MPU_Init();
mem2mem((uint16_t *)LED_Toggle,(uint16_t *)SDRAM_BASE_ADDR_CODE,400);
// LED_Toggle();
runCodeInSDRAM();
}