Are there Ethernet bootloaders available for LPC1700 and LPC2300/2400? If so, where can I find it?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Are there Ethernet bootloaders available for LPC1700 and LPC2300/2400? If so, where can I find it?

1,465 次查看
lpcware-support
Senior Contributor I

Ethernet bootloaders are available as part of the Flash Magic tool ( www.flashmagictool.com). After installing Flash Magic, you can find the bootloader in the Flash Magic\Ethernet Bootloader directory (C:\Program Files (x86)\Flash Magic\Ethernet Bootloader in a Windows x64 environment). An application note is available for download from www.nxp.com/documents/software/AN10744_Ethernet_Bootloader.zip

标签 (3)
标记 (3)
0 项奖励
回复
0 回复数