Is there any support in the SDK for the K70?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any support in the SDK for the K70?

749件の閲覧回数
dporada
Contributor III

I don't see any support for the tower board or the K70 processor in any of the SDK versions.  Is this a dying part?

ラベル(1)
2 返答(返信)

387件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Don,

K70 and K61 120 and 150MHz devices are not on the roadmap for support within KSDK.

Here is a link to see available devices and roadmap of support for the KSDK_v2 release.

Introducing Kinetis SDK v2

To date the plan is to retain the CodeWarrior/IAR/Keil support for those mature (not dying) products.  MQX4.2 also has the support for K70/K61.

Regards,

David

388件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hello Don,

at the moment there is no mention about K70 in future KSDK.

Please see below:

Introducing Kinetis SDK v2

Best Regards,

Iva

0 件の賞賛