I’m trying to write program that generates PWM output on PTD2 (J2-4) and RED LED is continually blinking .
My problem is with FlexIO register access. On the first “FLEXIO->…” instruction the program corrupts probably with unsupported NMI.
Sample program
// ========== RED LED Configuration
SIM->SCGC5 |= 0x2000; // enable clock to Port E
PORTE->PCR[31] = 0x100; // make PTE31 pin as GPIO for RED LED
PTE->PDDR |= 0x80000000; // make PTE31, output pin
PTE->PDOR |= 0x80000000; // turn off LED
// ========== FlexIO Configuration
FLEXIO->CTRL |= 0x0; // FlexIO disable
SIM->SCGC5 |= 0x80000000; // enable FLEXIO clock
PORTD-> PCR[2] = 0x600; // make PTD2 FXIO0 D2 (Alt. #6)
// PTD->PDDR |=0x4 ; // ???
FLEXIO->TIMCTL[0] |= 0x430202;
// Timer CTL: TRGSEL=0, TRIGPOL=0, TRGSRC=1,PINCGG=3, PINSEL=2, PINPOL=0, TIMOD=2
FLEXIO->TIMCFG[0] |= 0x0; // Timer 0 Config.
FLEXIO->TIMCMP[0] |= 0x58;
FLEXIO->CTRL |= 0x1;
已解决! 转到解答。
Thanks
It is working but only with FlexIO clock = MCGPCLK ( b01).
I tried also options with FlexIO clock = MCGIRCLK (which by default is 8MHz and can be divided), but there is no output on selected Timer output (PTD2).
Is it somehow connected to gated clock, if yes how to enable this clock ?
Regards
Shaul
Hello Rong
The problem with FlexIO clock = MCGIRCLK was solved there is MCG_C1 register with IRCLKEN field which enables IRC8M module.
Thanks for your helpful and fast response support.
Hope to hear from you with my next questions.
BR
Shaul
Hi, Shaul,
I suppose you have to enable the FlexIO gated clock before you access any FlexIO register. For your case, pls put the line
SIM->SCGC5 |= 0x80000000; as first line.
In other words, use the code like:
// ========== FlexIO Configuration
SIM->SCGC5 |= 0x80000000; // enable FLEXIO clock
FLEXIO->CTRL |= 0x0; // FlexIO disable
PORTD-> PCR[2] = 0x600; // make PTD2 FXIO0 D2 (Alt. #6)
// PTD->PDDR |=0x4 ; // ???
FLEXIO->TIMCTL[0] |= 0x430202;
// Timer CTL: TRGSEL=0, TRIGPOL=0, TRGSRC=1,PINCGG=3, PINSEL=2, PINPOL=0, TIMOD=2
FLEXIO->TIMCFG[0] |= 0x0; // Timer 0 Config.
FLEXIO->TIMCMP[0] |= 0x58;
FLEXIO->CTRL |= 0x1;
Hope it can help you
BR
XiangJun Rong
Hello Rong
I forgot to inform you that I’m using FRDM-KL43Z4 board with KDS v3.2 and KSDK v2.
I think that the problem is that with the “Build” process which generates hard fault during run time.
Unfortunately I’m not skilled enough to handle this kind of problems.
BR
Shaul
Hi, Shaul,
I am sorry. I think you have to select the FlexIO clock source with FLEXIOSRC bits in SIM_SOPT2, the default is 2b'00, which disable any clock.
BR
Xiangjun Rong
FlexIO Module Clock Source Select
Selects the clock source for the FlexIO transmit and receive clock.
00 Clock disabled
01 IRC48M clock
10 OSCERCLK clock
11 MCGIRCLK clock
Thanks
It is working but only with FlexIO clock = MCGPCLK ( b01).
I tried also options with FlexIO clock = MCGIRCLK (which by default is 8MHz and can be divided), but there is no output on selected Timer output (PTD2).
Is it somehow connected to gated clock, if yes how to enable this clock ?
Regards
Shaul
Hi,
I suppose that you do not enable PORTD gated clock because of using PORTD-> PCR[2] = 0x600;, pls use the code:
SIM->SCGC5 |= 0x3000; //enable PORTE and PORTD
Hope it can help you
BR
XiangJun Rong