Which SDK sample should I generate?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which SDK sample should I generate?

跳至解决方案
1,070 次查看
tedwu1
Contributor III

Hi friend,

We have a project that requires a CAN bus interface. I have installed the MCUXpresso IDE and have a FRDM-KW38 evaluation board. Now I want to generate an SDK sample. But I can't find the CAN bus project in driver_examples. I want to know which SDK example contains CAN bus procedure.

Thank you in advance.

Ted Wu

0 项奖励
回复
1 解答
1,053 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @tedwu1

The FlexCAN module is a communication controller that implements CAN protocol. You can find some useful demo applications for this module in driver_examples > flexcan from the KW38 SDK.
EduardoZamora_0-1701189103084.png

Regards,
Eduardo.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,054 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @tedwu1

The FlexCAN module is a communication controller that implements CAN protocol. You can find some useful demo applications for this module in driver_examples > flexcan from the KW38 SDK.
EduardoZamora_0-1701189103084.png

Regards,
Eduardo.

0 项奖励
回复