Which SDK sample should I generate?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which SDK sample should I generate?

跳至解决方案
2,805 次查看
tedwu1
Contributor III

Hi friend,

We have a project that requires a CAN bus interface. I have installed the MCUXpresso IDE and have a FRDM-KW38 evaluation board. Now I want to generate an SDK sample. But I can't find the CAN bus project in driver_examples. I want to know which SDK example contains CAN bus procedure.

Thank you in advance.

Ted Wu

0 项奖励
回复
1 解答
2,788 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @tedwu1

The FlexCAN module is a communication controller that implements CAN protocol. You can find some useful demo applications for this module in driver_examples > flexcan from the KW38 SDK.
EduardoZamora_0-1701189103084.png

Regards,
Eduardo.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,615 次查看
Larisabrownb
Contributor I
We'll break down specific SDKs across software categories, including CRM, file storage, marketing automation, and HRIS.SDK generation is computers writing code for you. A  love language test tool takes an API specification, and generates code that can be used to access that API. The SDK code is generated in the programming languages of your choice.SDKs usually contain some basic ingredients: documentation, code samples, APIs, programming tools, a debugger and more. SDKs are designed to allow developers to create applications on specific platforms, such as using an iOS or Android SDK.
 
0 项奖励
回复
2,789 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @tedwu1

The FlexCAN module is a communication controller that implements CAN protocol. You can find some useful demo applications for this module in driver_examples > flexcan from the KW38 SDK.
EduardoZamora_0-1701189103084.png

Regards,
Eduardo.

0 项奖励
回复