I can not connect to the HVP-MC3PH-Kit (High-Voltage Development Platform|NXP )!
Are the circuit boards (HVP-KV46F150M) not programmed with #ACIM KMS software?
How do I have to proceed to connect?
I would really appreciate some help! Thanks,
Roberto
Solved! Go to Solution.
The KV46 that you have probably does not have KMS install on the MCU.
I would recommend you use the ACIM Reference Design link here.
If you need KMS I will have to ask you to send the MCU card to me for re-programming or you can buy one from NXP.com HVP-KV46F150M - High-Voltage Development Platform Controller Card, Kinetis V MCU, KV46, 150 MHz
Best Regards,
Philip
The KV46 that you have probably does not have KMS install on the MCU.
I would recommend you use the ACIM Reference Design link here.
If you need KMS I will have to ask you to send the MCU card to me for re-programming or you can buy one from NXP.com HVP-KV46F150M - High-Voltage Development Platform Controller Card, Kinetis V MCU, KV46, 150 MHz
Best Regards,
Philip
I ordered a new PCB from NXP and it works with it now.
Thank you!