Problem connecting HVP-KV46F150M (HVP-MC3PH) with KMS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem connecting HVP-KV46F150M (HVP-MC3PH) with KMS

Jump to solution
1,548 Views
roberto_foelix
Contributor II

I can not connect to the HVP-MC3PH-Kit (High-Voltage Development Platform|NXP )!
Are the circuit boards (HVP-KV46F150M) not programmed with #ACIM KMS software?
How do I have to proceed to connect?

HVP-Error.jpg

HVP-KV46F150M.JPGHVP-MC3PH.JPG

I would really appreciate some help! Thanks,

Roberto

Labels (1)
0 Kudos
Reply
1 Solution
1,317 Views
philip_drake
NXP Employee
NXP Employee

The KV46 that you have probably does not have KMS install on the MCU.  

I would recommend you use the ACIM Reference Design link here.

If you need KMS I will have to ask you to send the MCU card to me for re-programming or you can buy one from NXP.com HVP-KV46F150M - High-Voltage Development Platform Controller Card, Kinetis V MCU, KV46, 150 MHz

Best Regards,

Philip

View solution in original post

0 Kudos
Reply
2 Replies
1,318 Views
philip_drake
NXP Employee
NXP Employee

The KV46 that you have probably does not have KMS install on the MCU.  

I would recommend you use the ACIM Reference Design link here.

If you need KMS I will have to ask you to send the MCU card to me for re-programming or you can buy one from NXP.com HVP-KV46F150M - High-Voltage Development Platform Controller Card, Kinetis V MCU, KV46, 150 MHz

Best Regards,

Philip

0 Kudos
Reply
1,317 Views
roberto_foelix
Contributor II

I ordered a new PCB from NXP and it works with it now.

HVP-KV46F150M-KMS.JPG
Thank you!

0 Kudos
Reply