Hello andreas,
No. Kinetis M series are not supported in KDS because are not supported by KSDK.
So KDS and KSDK are released together and KDS supports just devices that are currently supported by KSDK.
Best Regards,
Iva
hello Iva
then not have proccess expert for kinetis M, either CW10.6 or kinetis dising IDE
thanks
andres
Hi andres baena,
do you need work with PE or not?
What are you using for MCU?
Best Regards,
Iva
hi iva
i am using the MCU MKM33Z64ACLH5,
i do not understand,if work with PE or not
thanks
andres
Hi andres baena,
list of supported devices you find at your current version of CW C:\Freescale\CW MCU v10.6\MCU\ProcessorExpert in file README.txt
If I look at README.txt for 10.6.3 version, I don´t see support for KMx family.
You can check it in the newest version CW,
New CodeWarrior for MCU v10.6.4 available
I hope this helps,
Have a nice day,
Iva
Hi Iva Dorazinova,
I wonder if Freescale is going to add the KMx family to the PE and if .... when???
I really want to be sure before I start building my own HAL that will occupy me quite a time...
PE is an great USP for the Freescale micros!
Thanks in advance for your comment
Mark
Hello Mark,
actually coming soon TWR-KM34Z75M for KM family as Standalone version (unfortunately no support for MKM33Z64ACLH5),
after Eclipse Update you will see in KDS IDE:
but either for this case unfortunately is no PEx support.
Sorry for any inconvenience this may cause.
Best Regards,
Iva
hello
i am don't understand why this place, if it is not supported
There will be an update coming out these days supporting KM14, KM33 and KM34 with bare metal projects.
I'll post here a note once it is available for download.
Erich
hi Eric
i need to know, the data to download it.
thanks
Hi Andres,
see Support for Kinetis M (KM14, KM33, KM34) in Kinetis Design Studio
I hope this helps,
Erich
hi Erich
thank for you help.