ezPort on Kinetis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ezPort on Kinetis

4,985件の閲覧回数
colonel_panic
Contributor I

Hi.

 

Is there a document anywhere which describes the ezPort protocol as implemented on the Kinetis family ?

 

P.

5 返答(返信)

1,039件の閲覧回数
mnorman
NXP Employee
NXP Employee

There is an EzPort chapter in the Reference Manual for each Kinetis device.  In the case of the K60 100MHz 144 pin parts, the EzPort is described in chapter 30:  K60P144M100SF2RM

 

The datasheets contain the timing specifications/requirements.  e.g. K60P144M100SF2

 

-mnorman

1,039件の閲覧回数
robertofrechill
Contributor III

Hi, I´m developing the EZport programming with my Kinetis K20, I need information about what kind of file I must to charge by EZport and how I can transform my code file in this file.

Thanks.

Roberto

0 件の賞賛

1,039件の閲覧回数
santiago_gonzal
NXP Employee
NXP Employee

Hello Roberto,

Have a look here:

Downloading an s19 file Using the

EzPORT Module on the MCF521x

ColdFire® Microcontroller.

http://www.freescale.com/files/32bit/doc/app_note/AN3897.pdf

The file you need to generate is a binary s19 file.

Regards.

0 件の賞賛

1,039件の閲覧回数
robertofrechill
Contributor III

thanks!

Regards

0 件の賞賛

1,039件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi ,

Have you seen this AN?

AN4406 
AN4406, KwikStik-based EzPort programmer - Application Notes

Luis

0 件の賞賛