does the keaz128 can use the freemaster though the can channle?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

does the keaz128 can use the freemaster though the can channle?

ソリューションへジャンプ
607件の閲覧回数
xiaochenqiang
Contributor II

In the cw10.6, Only sci and bdm can are avialible for the components of freemaster? I want know that does the keaz128 can use the freemaster though the can channle?

thans!

ラベル(1)
タグ(1)
0 件の賞賛
1 解決策
467件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Yes, it seems Freemaster component in PE in CW and KDS only support SCI and BDM. You have to port Freemaster CAN driver by yourself. There is a DOC in community make the step very clear. You can refer to it.

https://community.nxp.com/docs/DOC-341890 

Regards,

Jing

元の投稿で解決策を見る

2 返答(返信)
468件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Yes, it seems Freemaster component in PE in CW and KDS only support SCI and BDM. You have to port Freemaster CAN driver by yourself. There is a DOC in community make the step very clear. You can refer to it.

https://community.nxp.com/docs/DOC-341890 

Regards,

Jing

467件の閲覧回数
xiaochenqiang
Contributor II

Hi Jing Pan,Thank you for your reply!

0 件の賞賛