Hi all,
I compile and run the cmsis_dspi_edma_transfer example with my NXP MK64FN1M0VLQ12.
One issue is found that CS becomes high after sending each bytes of data over SPI.
While using other examples, such as edma_b2b_transfer, or dspi_interrupt, everything works fine.
No clue about where and why the CS was pulled up during each bytes.
Thanks
Kevin
This chip select pin issue was fixed by implementing our own DSPI_EdmaTransfer function.
Wish fsl spi edma driver can use default configure in the future, so that user can pass down the flags we want.
In fsl_dspi_cmsis.c, the CS works as expected if I append PcsContinous as below:
static int32_t DSPI_EdmaTransfer(const void *data_out, void *data_in, uint32_t num, cmsis_dspi_edma_driver_state_t *dspi)
{
....
xfer.configFlags = kDSPI_MasterCtar0 | RTE_SPI0_MASTER_PCS_PIN_SEL | kDSPI_MasterPcsContinuous;
...
}
But this solution needs to change standard FSL K64 SDK... , and to make my code work, I have to tell build engineer to change their SDK file also. Any better way to manager this?
This fsl_dspi_cmsis driver should allow application to pass the flags down to it for flexible control.
Kevin
Hi Kevin,
There is a control bit SPIx_PUSHR.CONT selects a continuous selection format. The bit enables the selected PCS signals to remain asserted between transfers. In cmsis_dspi_edma_transfer, it doesn't set this bit. If you want to keep PCS low during frames, you can set isPcsContinuous to 1.
Regards,
Jing