Hi
I wanted to know if the CAN present in FRDM-KE06Z supports
1) 29 bit ID frame
2) CAN-FD (CAN with Flexible Data rate)
3) Is it possible for this board to communicate with K60 series using CAN?
Kind Regards
Amit
已解决! 转到解答。
Thank you for your interest in Freescale Kinetis product, I would like to provide service for you!
1: Yes, KE06 supports 29bit ID frame by setting the ID extended bit in the according register.
About details, please check the KE06 reference manual.
2: KE06 have MSCAN module, it is implementing the CAN 2.0A/B protocal, it isn't the CAN-FD.
3. If you want to using CAN communicate the KE06 with K60, you should use the CAN bus Transceivers.
Wish it helps you!
If you still have question, please let me know!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for your interest in Freescale Kinetis product, I would like to provide service for you!
1: Yes, KE06 supports 29bit ID frame by setting the ID extended bit in the according register.
About details, please check the KE06 reference manual.
2: KE06 have MSCAN module, it is implementing the CAN 2.0A/B protocal, it isn't the CAN-FD.
3. If you want to using CAN communicate the KE06 with K60, you should use the CAN bus Transceivers.
Wish it helps you!
If you still have question, please let me know!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jingjing
Thanks for the quick response.
1. In FRDM_KE06Z board, The CAN trans-receiver is present i.e SN65HVD230D, I think that should do the job. What do you suggest?
2. What is the difference in MSCAN and CAN present in K60 uc?
Regards
Amit
Hi Amit Kumar,
1. Yes, you can use SN65HVD230D as trans-receiver.
2. FlexCan is more flexible than Mscan, the FlexCAN module contains much more sophisticated state machine than the MSCAN module.
FlexCAN can automatically respond to a remote frame.
About more details, please compare the features in the KE06 and K60 reference manual.
Wish it helps you!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------