Farnell/element14 part numbers and links are provided here:
Finally I decided to order them (2x5 dual line through hole 1.27mm pin header and 1.27 10pin one-to-one cable) via taobao.com to a local trader.
Pricing: 0.3 USD for pin header and 1USD for cable, for 1pcs.
Thanks for all your information.
Farnell/element14 part numbers and links are provided here:
Hi
in the reference manual you can find this statement:
Note that J6 is not-populated by default. A Samtec FTSH-105-02-F-D or compatible connector can be added to the J6 through-hole connector. A mating cable, such as a Samtec FFSD IDC cable, can then be used to connect from the OpenSDA of the FRDM-KL25Z to an off-board SWD connector.
so I would recomend to contact SAMTEC!
Pavel
First of all Samtec product FTSH-105-02-F-D is not available from element14 any more. And I found other similiar products are very exepensive for a connector. It seems I have to find it in China anyway.
Hi
In case you need few pieces, you can order free samples directly in the Samtec webpage. For connectors and cables.
I have ordered some FFSD-05-D-06.00-01-N/FFSD-10-D-06.00-01-N cables, and FTSH-105-02-F-D pin headers.
I hope it helps.