Unexplained Acronyms. What does FTFA mean?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unexplained Acronyms. What does FTFA mean?

1,230 Views
admin6
Contributor III

It would be insightful if NXP would kindly grant someone time to document the LITERAL meaning of the unexplained acronyms that are FREQUENTLY used in all documentation for MCUs such as the KL27z, especially the reference manual and datasheets.

For example,  what to the letters "FTFA" mean in FTFA_FOPT.  Just stating that it "refers" to the Flash Memory Module is not good enough. Why is it not called the FMM then?

Without knowing what the letters stand for it is impossibly hard to learn or sensibly guess or re-construe the name of some MCU modules.

It would be insightful if there was a glossary of such terms at hand.

Here are some explanations that might help others;

Acronym Decoder (basic but a good effort - please give it a like if you find it useful)

Acronym Decoder 

Arm Glossary  (e.g.   AMBA =  Advanced Microcontroller Bus Architecture)

Support | Arm Glossary – Arm Developer 

AIPS explanation  (e.g  AIPS = AMBA to IPS bridge.  Or AHB to IPS bridge.)

"The AMBA to IP Bus Bridge (AIPS) module provides an interface between the 32-bit high speed StandardProduct          Platform (SPP) bus and the lower bandwidth 32-bit Intelligent Peripheral Subsystem (IPS) bus."

https://www.nxp.com/docs/en/reference-manual/MAC7100RM.pdf 

FTFA explanation?   (FTFA = Flash TFA.    TFA = Trusted Firmware-A)   (Seriously?)

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev19.09.pdf 

0 Kudos
Reply
1 Reply

1,129 Views
mjbcswitzerland
Specialist V

Hi

I suspect FTFA means something like Flash-Thin-Film (type) A
and FTFL and FTFE types L and E:

https://www.nxp.com/docs/en/application-note/AN4835.pdf 

Regards

Mark

[uTasker project developer for Kinetis and i.MX RT]