USB drivers working previously with K50 family stop working on MK20DX128VLF5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB drivers working previously with K50 family stop working on MK20DX128VLF5

1,070件の閲覧回数
maximosipov
Contributor I

After USB reset and first descriptor exchange DFN8 error is generated by the USB controller (device mode).

Error is observed on both USB Stack http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB&fpsp=1&tab=Design_Tools_Tab and K20 Freedom board USB CDC code.

Any hint on this issue? Working CDC code or recommendations on workarounds are highly appreciated.

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

867件の閲覧回数
maximosipov
Contributor I

Hi,

First of all, mcuoneclipse is amazing and CDC driver is very cool. Unfortunately didn't help in my case, so I suspect a hardware problem - either in chip or layout (however layout is trivial)...:smileysad:

Regards,

Max

0 件の賞賛
返信

867件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Maxim,

Have you tested the CDC example that Erich Styger sent you, but using a FRDM-K20D50M board?

I just tested it and it worked properly. If you are getting troubles with your custom hardware, have you ensured if you are using the same crystal value than FRDM-K20D50M board (8 MHz), in order to have a valid clock initialization?

Hope this will be useful for you.

Best regards!

/Carlos

0 件の賞賛
返信

867件の閲覧回数
maximosipov
Contributor I

Thank you - I checked USB clock as a very first step, on USB data lines - it all correct. So only HW options left.

0 件の賞賛
返信

867件の閲覧回数
Monica
Senior Contributor III

Hello Maxim,

was this example useful? Please keep us posted, we'd like to know :smileywink:

Best,

Monica.

0 件の賞賛
返信

867件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Maxim,

attached is an example I'm using.

See USB CDC with the FRDM-K20D50M | MCU on Eclipse

Erich

0 件の賞賛
返信