I'm trying to use FRDM-K82F, and fllow the step from "http://www.nxp.com/products/software-and-tools/run-time-software/kinetis-software-and-tools/ides-for...":
3.2 Build, Run and Debug SDK Examples->Use Kinetis Design Studio->4. Run a Demo Application.
When I Drag and drop the "JLink_OpenSDA_V2_1_2015-10-13.bin" file into the bootloader drive, the operation is failed and FRDM-K82F couldn't poweron.
Any suggestions for how to find/fix the problem?
Thanks,
Zahom
解決済! 解決策の投稿を見る。
Hi Zahom,
Thanks for your reply.
I'd highly recommend that you can use the multmeter to check the hardware circuit of the board according to the its sch.
http://cache.nxp.com/files/32bit/hardware_tools/schematics/FRDM-K82F-SCH.pdf
Hope it helps.
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
zahomz I'm facing the same problem. Please help. the K82 freedom board doesn't power up. No lED glows. I'm unable to enter the bootloader mode.
I checked with multimeter, the board is getting +5V from the usb.
Please help
Hi, Rushiraj,
I haven't solve my problem, but finally I use JLink to program the k82 by SWD.
Hope this could help you!
zahomz You use JLink means?
Are you using the JLink JTAG Debugger?
It costs a lot I cannot buy that debugger. :smileysad:
Hi Zahom,
I've attached the JLink_OpenSDA_V2_1.bin, please try it when you force the OpenSDA interface into the bootloader driver again.
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, jeremyzhou,
Thanks for your help. But because of the problem, my board couldn't poweon now. How could I resolve this problem? (Windows couldn't find the bootlader drive.)
Hi Zahom,
Thanks for your reply.
I'd highly recommend that you can use the multmeter to check the hardware circuit of the board according to the its sch.
http://cache.nxp.com/files/32bit/hardware_tools/schematics/FRDM-K82F-SCH.pdf
Hope it helps.
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, jeremyzhou,
I haven't resolve this problem, but I use j-link to program the flash now.
Thanks for your help!