The problem of collecting the internal temperature of K66 ADC.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The problem of collecting the internal temperature of K66 ADC.

903 次查看
jetli
Contributor II

Recently,My Project(Kinetis K66) need using the ADC capture pin voltage and internal CPU temperature.Project ADC acquisition sequence is the first collection of pin voltage, and then capture the temperature, reciprocating cycle.When I do not pick any voltage source on the pin , the acquisition temperature is normal(16bit adc value 6545).But if I pick voltage source on the pin , the acquisition is mistake(16bit adc value 16254).I don't why? Somebody who can help me?

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

746 次查看
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear jet li,

Can you give me more information or send me your project to have a better understanding of the problem.

Best regards.

Jonathan.

746 次查看
jetli
Contributor II

Dear Jonathan lglesias,

      After your company's technical staff to help, I found reason is ADC input frequency is too high, resulting in interference between the channels, and now has been working very well, thank you!

Best regards.

jet li;

0 项奖励
回复