i am trying to port fatfs to Sd card.
i refer this link https://community.nxp.com/docs/DOC-330958
now my question is that which file i need to added in my project
because in main() function no any spi related function are call.
assign to @TIC kerry
已解决! 转到解答。
Hello Arth Shah,
Thanks a lot for your patient.
Just as you send me the message, you need the KDS SD Fatfs project for KL25, and you refer to my post before which just have MDK project.
Now, I already help you finished the KDS project, the same board as my own post which you already give the link, the KDS project is working OK on my side, you can refer to the attachment.
The project can be find in folder: SD_FatFS-KL26Z_KDS\boards\frdmkl26z\demo_apps\hello_world\kds
When you open the KDS IDE, just select the workspace path in : SD_FatFS-KL26Z_KDS
This is the test result:
Com print information:
SD card information:
Wish it helps you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
Any FAT SD card solution can be used also as a low level sector read/write interface.
You still need to switch the card into SPI mode (the first part of SD card mounting) but after you can read and write sectors however you like.
Regards
Mark
Hi
Here is a very short video that I have made for you showing reading and writing RAW sectors: https://youtu.be/VY-I0_h5p4Q
You can get this form the open source uTasker project at http://www.utasker.com/kinetis.html which contains all needed for SD card operation as well as complete operation simulation. If you are no interested in a complete working solution you can simply use VS to step through all code to see how it works and then copy the bits that are of interest.
SPI interface details are in the first chapters of http://www.utasker.com/docs/uTasker/uTasker_utFAT.PDF
Regards
Mark
Hello Arth Shah,
Thanks a lot for your patient.
Just as you send me the message, you need the KDS SD Fatfs project for KL25, and you refer to my post before which just have MDK project.
Now, I already help you finished the KDS project, the same board as my own post which you already give the link, the KDS project is working OK on my side, you can refer to the attachment.
The project can be find in folder: SD_FatFS-KL26Z_KDS\boards\frdmkl26z\demo_apps\hello_world\kds
When you open the KDS IDE, just select the workspace path in : SD_FatFS-KL26Z_KDS
This is the test result:
Com print information:
SD card information:
Wish it helps you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Arth Shah,
Comment the Fatfs code, just leave MMCinit(),
Main code like this:
int main(void)
{
char ch;
unsigned int i,j;
FATFS fs;
FRESULT fr;
FIL fil;
UINT bw;
char file_name1[12]="Test.csv";
char file_name2[12]="Test.txt";
/* Init board hardware. */
BOARD_InitPins();
BOARD_BootClockRUN();
BOARD_InitDebugConsole();
PRINTF("hello world.\r\n");
spiInit(Master);
MMCInit();
/*
fr= f_mount(&fs,file_name1,0);
if(fr)
{
PRINTF("\nError mounting file system\r\n");
for(;;){}
}
fr = f_open(&fil, file_name1, FA_WRITE | FA_OPEN_ALWAYS);//н¨csvÎļþ
if(fr)
{
PRINTF("\nError opening text file\r\n");
for(;;){}
}
fr = f_write(&fil, "Test1 ,Test2 ,Test3 ,Test4 \r\n", 29, &bw); //±íÍ·
if(fr)
{
PRINTF("\nError write text file\r\n");
for(;;){}
}
fr = f_close(&fil);
if(fr)
{
PRINTF("\nError close text file\r\n");
for(;;){}
}
fr= f_mount(&fs,file_name2,0);
if(fr)
{
PRINTF("\nError mounting file system\r\n");
for(;;){}
}
fr = f_open(&fil, file_name2, FA_WRITE | FA_OPEN_ALWAYS);//н¨txtÎļþ
if(fr)
{
PRINTF("\nError opening text file\r\n");
for(;;){}
}
fr = f_write(&fil, "Test1 ,Test2 ,Test3 ,Test4 \r\n", 29, &bw); //±íÍ·
if(fr)
{
PRINTF("\nError write text file\r\n");
for(;;){}
}
fr = f_close(&fil);
if(fr)
{
PRINTF("\nError close text file\r\n");
for(;;){}
}
*/
while (1)
{
//ch = GETCHAR();
// PUTCHAR(ch);
for(i=0;i<10;i++) for(j=0;j<65535;j++);
printf("\ntest_sd\n");//
}
}
Debug again, where you stop?
This is my debug picture:
You can see, even I didn't insert the SD card, the SPI also can send data.
But take care, if your SD card can't give feedback. It may caused by the SD card, this code just for SD2.0 card.
You can debug the MMCInit, and check where it can run, whether CMD0 have feedback.
Besides, also refer to my post, check your SD card hardware circuit.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hello kerry,
i want to tell you something,
i have one new project created by me before some week from link provided by you
today i try this project.
unfortunately this project is work but not for all .sometimes it's work or sometimes not.
please check this code on your side please.
Hi Arth Shah,
I think you also need to check the hardware, the SPI wire between the MCU and your SD card.
If there has a lot of distrub in the wire, it may cause the problem.
You can check your SPI bus wave, the SPI line should not long, it should as short as possible.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Arth Shah,
Give me some picture of your board and SD card connection.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Arth Shah,
Thank you for your pictures.
Please divide all the wire which connect together, now you are using cable which connect all the SPI wire together.
Please divide it one by one, especial the SPI_CLK, SPI_MOSI, SPI_MISO, then try again.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hello kerry,
i try this one but still remain same problem on my code,
it's sometime work and sometime not work.
your code is not work still now.
and here i attach my debug picture of my code.
every time my code is stop here.
what's the problem in SPI?
Hi Arth Shah,
Try to modify my spiinit code, to add the internal port pull up.
void spiInit (uint8 bMode)
{
PORTC->PCR[4] |= PORT_PCR_MUX(1) | PORT_PCR_PE_MASK |PORT_PCR_PS_MASK;
PORTC->PCR[5] |= PORT_PCR_MUX(2) | PORT_PCR_PE_MASK |PORT_PCR_PS_MASK;
PORTC->PCR[6] |= PORT_PCR_MUX(2) | PORT_PCR_PE_MASK |PORT_PCR_PS_MASK;
PORTC->PCR[7] |= PORT_PCR_MUX(2) | PORT_PCR_PE_MASK |PORT_PCR_PS_MASK;
===========
I don't know whether your SD card board have the according external pull up or not, my SD card circuit have the external pull up resistor, so just enable the internal pull up and try again.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hello kerry,
thanks for the help
i had try to make internal pull up enable but still your code is not working on my board but my code is working completely now.
so i want to go ahed with this project
thank you so much for the help.
Hi Arth Shah,
I simply check your project, still the same structure with me.
Anyway, it's good to hear your can work on your board,
For the new question, please create a new question post about it, thank you !
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Arth Shah,
Run into MMCInit, then put break point in the following yellow line:
Can you run to this place?
Besides, what the board you are using now?
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------