Protoboard advice for FRDM-K64F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Protoboard advice for FRDM-K64F

跳至解决方案
923 次查看
olivierkieffer
Contributor II


I'm looking for a protoboard for FRDM-K64F. I know this board is compatible with Arduino headers, but I want to use CAN controller feature directly from K64 (not through SPI -Arduino- shield). As far as I understand the pinout, CAN Rx/Tx are available on the Freescale I/O headers but not on the Arduino headers, so I can't use Arduino protoboard.

I would need a prototoboard (to add a CAN transceiver and some other components)  with all Arduino and Freescale I/O headers available.

Any advice?

Thanks

0 项奖励
回复
1 解答
681 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Olivier,

Unfortunately, NXP hasn't provided some kinds of the protoboard just as you want, and I'd like to suggest that you can give a try on eBay.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
682 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Olivier,

Unfortunately, NXP hasn't provided some kinds of the protoboard just as you want, and I'd like to suggest that you can give a try on eBay.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
681 次查看
olivierkieffer
Contributor II

Hi Jeremy,

I did not find any 3rd party neither. I will just make my own board.

Thanks for your help.

Olivier

0 项奖励
回复